Shop-Trak Defining Main Parameters

Use the Main tab of the Shop-Trak Parameters form to specify the type of labor transactions to be collected, the options to display in Shop-Trak Shop Floor, and how materials will move between operations.  

To define Main parameters:

  1. Open the Shop-Trak Parameters form.
  2. Click the Main tab.
  3. Specify this information:

Available Menu Options

Quantities

Settings

Email Settings

File Locations

 

Available Menu Options

Specify which transaction types and option buttons will be available on the Labor, Materials, and Info tabs in Shop-Trak Shop Floor.  All or any combination of these options are valid.  These settings will apply to all users unless an Employee Profile has been set up for a specific user, which will override these settings.  

Labor:

Materials:

Info:

Quantities

Specify how quantities are moved between operations and between operations to stock.   

Operation to Operation Moves:
This parameter controls how quantities are moved between operations.  You can specify whether quantities can move automatically, whether employees can move quantities at the same time as they are completing quantities, or whether quantities can move manually with a WIP Move.

Operation to Stock Moves:
This parameter controls how quantities are moved to stock from the last operation of the job.  You can specify whether quantities can move automatically, manually, or with a WIP Move.  If using Lot, Location, or Serial Tracking, additional fields will also display within Shop-Trak Shop Floor.

Operation to Operation Moves

Operation to Stock Moves

Description

Automatic

Automatic

Allows quantities completed to be moved automatically to the next operation, and the last operation moves the quantities complete into stock.  The Moved field is not available for update.

Automatic

Manual

Allows quantities completed to be moved automatically to the next operation, while allowing the movement of quantities to stock to be entered manually. The Moved field will display the quantity complete on the last operation of the Labor transaction, but can be changed by the employee.

Automatic

WIP Move Transaction

Allows quantities completed to be moved automatically to the next operation, and requires the movement of quantities to stock using a WIP Move transaction.  The Moved field is not available for update.

Manual

Manual

Allows quantities completed to be moved manually to the next operation, including the last operation which moves the quantities to stock.  The Moved field will display the quantity complete, but can be changed by the employee.  

Manual

WIP Move Transaction

Allows quantities completed to be moved manually to the next operation, and requires the movement of quantities to stock using a WIP Move Transaction.  The Moved field can be updated on all operations except for the last.

WIP Move Transaction

WIP Move Transaction

Only a WIP Move transaction can move quantities between operations and into stock.  The Moved field is not available for update.

Entry of WIP Move Quantities:
This parameter enables or disables the WIP Move feature.  

Settings

Specify these fields in the Settings section.

Start Additional Allocation Basis:
This parameter defines how rates and time are allocated when an employee is working on more than one job at the same time using the Shop-Trak Shop Floor Start Additional Job transaction.

Show Job Summary:
This parameter determines whether to display a job summary window in Shop-Trak Shop Floor to assist employees in assigning the labor transaction appropriately.  Pertinent job information is displayed including quantities Received, Complete, Scrap, and Moved for each job and operation.

Attendance on Punchout:
This parameter determines whether to show the employee's Time Sheet Display report in Shop-Trak Shop Floor upon punching out for the day.  The Time Sheet Display summarize the employee's transactions for the day.  This allows the employee to confirm their transactions for manufacturing and payroll.

Display WIP Moves on Punchout:
This parameter determines whether or not to include WIP Move transactions on the employee's Time Sheet Display report.  Select Y (Yes) to display the WIP Move transactions or select N (No) to not display.

Indirect Labor Posting:  
This parameter determines how journal entries will be created for Indirect Labor transactions.  You can choose to create Shop-Trak Shop Floor journal entries when Indirect Labor transactions post, or create journal entries in the Payroll Distribution journal at the time payroll is posted.

Password Security:
This parameter determines if passwords will be required in Shop-Trak Shop Floor.  Passwords are defined on the Shop-Trak Employee Profile form for those employees requiring a password.

Week Ending Day:
This parameter applies to RTE Transaction validation.  Select the week ending day that employees must validate transactions through.  

Retain Employee Log:
Specify the number of days to retain the employee log tables.  You can retain the log tables for up to 999 days.  The employee log tables are:

NOTE:  Before specifying this field, you should take each table into consideration.

Unassigned Cost Codes:
When using the Infor SyteLine Project module, each transaction requires an associated cost code.  Select a cost code that will become the default value when performing a Project Labor transaction.  The default can be changed by the employee when starting the transaction.  The cost code must be a valid Infor SyteLine cost code.

Require Secure Logon:
This parameter allows you to specify if workstations will require a secure logon in order to access Shop-Trak Shop Floor.  This is essential in a click-once, or SaaS, environment to ensure that employees are actually logging in from a qualified network workstation.  If this option is checked, it will force each Shop-Trak Shop Floor workstation to be set up with a Workstation Profile.  The Workstation Profile determines which workstations in the domain can access a Shop-Trak Shop Floor session.  If this parameter is enabled and the workstation does not have a Workstation Profile, no access will be granted.  

Email Settings

This parameter is used in conjunction with the Kanban Replenishment feature.  When a Purchase Order or Job Order is created from a replenishment, an e-mail message can be sent to notify the proper personnel to take action.

Email Server:  Specify your Exchange Server name.

Email From:  Specify a valid e-mail address located on your Exchange Server that the messages will be sent "from."  For example, purchasing@yourcompany.com.

File Locations

Path to Button Images:
You can override the default Shop-Trak Shop Floor button images by specifying a path to the alternate images.  You can also override the default images at the employee level using the Shop-Trak Employee Profile form, which allows you to designate unique buttons for individual employees.

Shop-Trak first looks for button images using the path specified in the Path to Button Images field on the Shop-Trak Employee Profile form.  If the employee does not have a profile, or the field is blank, Shop-Trak then looks in the Path to Button Images field on the Main tab of the Parameters form.  If this field is blank, Shop-Trak will use the default image location initially installed with Shop-Trak.

To customize the Shop-Trak Shop Floor button images:

    1. Go to the Button-Images directory located in your Shop-Trak download.
    2. Copy the default JPG or BMP button image files to a shared UNC path.
    3. Replace the default images with your new images, keeping the default file names.
    4. Specify the shared UNC path in the Path to Button Images field.
    5. The new button images will then display in Shop-Trak Shop Floor.

Path to Employee Photos:  
Specify the shared UNC path to employee photo files.  The image files must be saved as <employeenumber>.bmp.  For example: 100.bmp.  The employee's photo will then display on the Shop-Trak Shop Floor workstation when the employee enters their employee number.  

  1. Save your changes and close the form.

NOTE:  The Shop-Trak version number installed on the database is displayed on the bottom of the Main tab.  This version number should always match the version number installed on the client.  The client version number is displayed when you select Help > About from Shop-Trak Shop Floor.   


Related Topics

Shop-Trak Parameters Form

Shop-Trak Single Transaction Costing

Shop-Trak Start Additional Transaction Costing

Shop-Trak Multi-Job Transaction Costing

Shop-Trak Team Transaction Costing

Shop-Trak Project Transaction Costing

Shop-Trak Work Center Labor Transaction Costing