To facilitate the migration of DataView definitions from one database to another, use the DataViews Import/Export utility to import and export DataViews. This can be done one DataView at a time or in mass. The utility can also be used as a tool to maintain back-ups of custom DataViews. The DataViews Import/Export form supports the function of exporting DataViews to an XML file and importing DataViews from a pre-formatted XML file. The XML file is saved in the directory specified following the naming convention WBDataViews_[DataViewName].xml.
Follow these steps to import or export a DataView:
DataView
Select a range of DataViews.
Group Name
Select a group name or range of names.
User Name
Select a user name or range of names.
Include Permissions
Select this check box to include permissions for each DataView being exported.
Include Layouts
Select this check box to include layouts for each DataView being exported.
The import does not allow a DataView to be added to a database if one of the same name already exists. Instead, copy the existing DataView to a new name in the target database then delete the duplicate record so it can be loaded without error.
If an error occurs during import, no elements of the DataView with the issue are loaded.
The import routine does not validate users or groups for permissions and layouts; users and groups must be added manually to the target database as needed.