WinStudio
Use the Input Mask property to specify a mask to apply to text entered into a component (such as a telephone number). A mask serves as a template or pattern for text.
Character |
Description |
|---|---|
> |
Digit placeholder (0-9). Prompt character is blank. Applies to numeric data types. |
9 |
Digit placeholder (0-9). Prompt character is 0. Applies to numeric data types. Masks with 9 do not support Null values (see Usage Notes). |
Z |
Digit placeholder (0-9). Prompt character is blank, and the thousands separator is not applied. Applies to numeric data types. |
< |
Digit placeholder for decimal positions (0-9). Prompt character is blank. Removes non-meaningful trailing zeros. Applies to numeric data types. |
# |
Digit placeholder (0-9). Prompt character is blank. Applies to numeric data types. NOTE: This is available only for backward compatibility and generally is not used. |
- |
Negative sign placeholder. Applies to numeric data types. |
. |
Decimal placeholder. This character is treated as a literal in the mask. Applies to numeric data types. The actual character used is the one specified in your regional settings (see Usage Notes). |
, |
Thousands separator. This character is treated as a literal in the mask. Applies to numeric data types. The actual character used is the one specified in your regional settings. You do not need to specify a thousands separator. |
: |
Time separator. This character is treated as a literal in the mask. Applies to the DATE data type. The actual character used is the one specified as a separator in your regional settings. |
A |
Alphanumeric character placeholder (0-9 and a-Z). Applies to the CHAR data type. |
? |
Alphabetic placeholder (a-Z). Applies to the CHAR data type. |
X |
Alphabetic placeholder that forces characters to capital letters (A-Z). Applies to the CHAR data type. |
x |
Alphabetic placeholder that forces characters to lowercase letters (a-z). Applies to the CHAR data type. |
& |
Character placeholder. Valid values for this placeholder are ANSI characters in the following ranges: 32-126 and 128-255. Applies to the CHAR data type. |
\ |
Literal escape. To treat any of the above characters as literals, use a backslash preceding the character. |
[NONE] |
Do not apply a mask. See Usage Notes. |
Suppressing Trailing Zeros For decimal values whose mask includes the < character, the value displays with non-meaningful trailing zeros removed.
If the mask is set to >>>>>9.99<<< and the user enters 12345.125000, the value displays as 12,345.125. This formatting takes place after the cursor leaves the field.
Underlying Type, WinStudio Component Property