WinStudio
Use the Round property to round and truncate decimal values to a specified number of digits to the right of the decimal position. The number of digits is specified in the Decimal Point Position property.
The property can be set for a component with a data type of Decimal, Currency, R4, or R8 and for which no input mask is defined.
A truncated digit greater than 5 in a component value rounds the value up.
| Setting | Description |
|---|---|
| True | Round and truncate a component's decimal value. |
| False | Default. Do not round or truncate a component's decimal value. |