WinStudio
IWSFormComponent interface
Sets or returns a string containing the internal value of an editable component.
If the component is bound to a property, then setting its internal value updates the property, marks the property modified, and notifies other dependents on the property (such as other components bound to it) to refresh.
object.TextInternal = string
Part |
Description |
object | Required. A reference to an editable component object. |
string | Required. The new value to be assigned to the component. |
object.TextInternal
Part |
Description |
object | Required. A reference to an editable component object. |
WinStudio stores the values of editable components as character strings.
In a tree component, this property returns the value of the first property in the current node.
With the exception of how date and numeric formats are presented, this property is the same as the Text property. For instance, with the Text property, dates are presented using the current locale display format. With this property, the date is presented using the WinStudio internal date format.
Sub Main() Dim oComponent As IWSFormComponent Dim value1 As String Dim value2 As String 'Show current field values: oComponent = ThisForm.Components("FirstGridCol") value1 = oComponent.TextInternal value2 = ThisForm.Components("SecondGridCol").TextInternal Application.ShowMessage("First column value: " _ & value1 & vbLf & "Second column value: " _ & value2) 'Swap values and display confirmation message: oComponent.TextInternal = value2 ThisForm.Components("SecondGridCol").TextInternal = value1 Application.ShowMessage("The text should now be swapped!") End Sub
NotifyDependentsToRefresh Method
SetCurrentObjectPropertyInternal Method
SetCurrentObjectPropertyModified Method
SetCurrentObjectPropertyPlusModifyRefreshInternal Method
SetObjectPropertyInternal Method
SetObjectPropertyModified Method
SetObjectPropertyPlusModifyRefreshInternal Method