WinStudio
IWSIDOCollection interface
Refreshes an object property in a specified IDO collection.
object.NotifyDependentsToRefresh( string )
Part |
Description |
| object | Required. A reference to a valid IDO collection object. |
| string | Required. The name of the object property.
NOTE: If the string is empty (""), all properties are refreshed. |
Sub Main()
Dim vEcnitemType As String
Dim bCostView As Boolean
If ThisForm.PrimaryIDOCollection.IsCurrentObjectNew Then
vEcnitemType = Left(ThisForm.PrimaryIDOCollection.GetCurrentObjectProperty("EcnitemType"), 1)
Select Case vEcnitemType
Case "C"
bCostView = ThisForm.Variables("vCanStdViewCosts;").Value = "1"
Case "J"
bCostView = ThisForm.Variables("vCanJobViewCosts").Value = "1"
Case "E"
bCostView = ThisForm.Variables("vCanEstViewCosts").Value = "1"
End Select
If bCostView Then
ThisForm.PrimaryIDOCollection.CurrentItem("DerMatlCostConv"). _
SetValue(ThisForm.PrimaryIDOCollection.CurrentItem.Properties("MatlCostConv"))
ThisForm.PrimaryIDOCollection.NotifyDependentsToRefresh("DerMatlCostConv")
ThisForm.PrimaryIDOCollection.CurrentItem("DerLbrCostConv"). _
SetValue(ThisForm.PrimaryIDOCollection.CurrentItem.Properties("LbrCostConv"))
ThisForm.PrimaryIDOCollection.NotifyDependentsToRefresh("DerLbrCostConv")
ThisForm.PrimaryIDOCollection.CurrentItem("DerFovhdCostConv"). _
SetValue(ThisForm.PrimaryIDOCollection.CurrentItem.Properties("FovhdCostConv"))
End If
End If
End Sub
SetCurrentObjectProperty Method
SetCurrentObjectPropertyModified Method
SetCurrentObjectPropertyPlusModifyRefresh Method
SetObjectPropertyModified Method
SetObjectPropertyPlusModifyRefresh Method