Adding or Updating Customer Credit Card Information

When you add a customer's credit card information in your system, you can choose to store the information for reuse on later orders by that customer. You can store information about multiple credit cards for one customer, using different Ship To addresses for the customer.

Adding Credit Card Information

To add credit card information for a customer:

  1. (Optional) From the Customer Orders, Service Orders, A/R Posted Transaction Summary, or  A/R Posted Transaction Detail forms, click Pay with Credit Card to display the Credit Card Payments form.
  2. Use the Credit Card Payments form to enter customer credit card information that will be used to pay the invoice when it is generated.
    Note: A customer's credit card information can also be entered remotely, from the Service Management Mobile application or a Customer Portal.  

    Specify this information. (If this form is called from another form, relevant information is already filled in.)

    Customer

    Specify the customer number.

    Ship To

    Specify the customer Ship To address (also known as the Customer Sold To location). If the field is left blank, the zero Ship To address is used.

    Name

    The customer name is displayed.

    Transaction Type

    Specify the action to be requested from the credit card processing software:

    Note: The authorization process submits a charge for the either a fixed amount or a percentage of the sale based on the credit card interface parameter setting.

    Ship Method

    Select a ship method to calculate the freight (shipping) charges for this credit card order and include that in the Total Amount. See  Setting Up Shipping Charges for Credit Card Customers. This field is optional. If you leave it blank, you must use standard SyteLine procedures to calculate the freight charges. (For orders placed through the Customer Portal, this field is display-only and shows the ship method selected by a Customer Portal user when placing a credit card order.) This field is enabled only when Transaction Type is Authorize and Reference Type is Customer Order.

    Total Amount

    Specify the total amount to be invoiced. If you specified a Default Authorization method on the Credit Card Parameters form, a calculated amount is filled in automatically for pre-authorizations.  See  Pre-authorizing Credit Card Amounts or Percentages.

    Reference

    Specify the reference to which the credit card should be applied:

    Customer Reference

    Specify the name of the customer or individual who authorized the credit card transaction. This value is provided by the customer, typically to track the employee or representative in their organization who authorized the transaction. This reference is mainly used for business, corporate or government GSA purchasing cards. This value can be passed to the third-party credit card system to qualify for Level 2 or 3 reporting.

    Card Number

    If you use the CenPOS gateway, either:

    If you use another gateway, specify the 16-digit number listed on the front of the customer's credit card. If the credit card has been used and stored by the customer previously, you can select the number from the drop-down list.

    Note: The credit card number is not stored locally; it is transmitted only for authorization purposes.

    Store for Future Orders

    If you use the CenPOS gateway, you can select this field even for a blank credit card number.  Credit card information is entered through the CenPOS virtual terminal; a token ID is stored locally for reference. When you authorize and submit the credit card information to CenPOS, SyteLine creates an entry in the Customer Credit Cards form.

    If you use another gateway, select this option to save the information in the back end system for future use. The actual card number is not saved in the system; only a pointer to the information in the third-party system is saved. When you click Process,SyteLine creates an entry in the Customer Credit Cards form.

  3. For security purposes, only the last four digits of the credit card number are stored. A reference to the third-party credit card processing application, where the full credit card number is securely stored, is used to access the full credit card number during processing.

    Expiration Date

    Specify the card expiration date in the form MM/YY. For CenPOS, this field is not available.

    Name on Card

    Specify the card holder's name exactly as it appears on the credit card. For CenPOS, this field is not available.

    CV Number

    Specify the 3-digit security number on the back of the card. For CenPOS, this field is not available.

    Street, City, Prov/State and Postal/Zip

    Specify the billing address information for the card holder.

  4. If you use the CenPOS gateway, click Authorize to display the Credit Card Web Payment form with the CenPOS virtual terminal.  Here you specify the card number, expiration date, name on the card, last four digits, and optionally an email address. If the card was previously saved for this customer, the information is already filled in. If this form is associated with an order, the invoice number is filled in. Click Submit to send the information to CenPOS; then click OK to close the Credit Card Payments form.

    If you use another gateway, click Process to send the completed information to the third-party system where it can be authorized.

If You Try to Perform a Second Authorization

To prevent additional fees, if you try to perform a second authorization against an order, a warning message is displayed to confirm the request. Click Yes to confirm or No to deny the reauthorization.

Changing Credit Card Information

To change stored credit card information for a customer:

  1. In the Customer Credit Cards form, delete the existing record.
  2. In the Credit Card Payments form:

A new Customer Credit Cards record is created and stored.


Related Topics

Processing Customer Credits/Returns on Credit Cards

Pre-authorizing Credit Card Amounts or Percentages

Reauthorizing a Credit Card upon Shipment

About the Credit Card Interface