Working with Notes

You can annotate a record or a collection of records by attaching one or more notes. This topic includes information about:

The See Also link at the top of this page points to other topics that explain how to create, view, and attach/detach notes.

Object and Class Notes

The system allows you to create:

You can attach multiple notes, of either type, to a record. Once you attach a note of any type to a record, all other users of the system can read the note.

When you attach a note, the status bar displays the word NOTES, and the Actions menu displays a check mark next to the Notes for Current option (for single-record notes) or next to the Notes for All option (for notes attached to the whole collection).

NOTE: Some forms use application-specific notes instead of the standard Object Notes and Class Notes. These notes are similar in purpose but different in use from the standard notes. For details about the application-specific notes, see Notes Form (Modal).

Reusable Notes

Reusable notes are defined on the System/User Notes form. You can create these notes once and attach them multiple times, either as object notes or class notes. There are two kinds of reusable notes:

Internal/External Notes

All notes can also be classified as either external or internal notes. If you select the Internal check box for a note, the system tags it as an internal note. Otherwise, the system treats the note as an external note. This classification is used when printing notes in reports, as described below.

Printing Notes in Reports

Many reports and utilities allow you to specify what kinds of notes can be printed as part of the output. Sometimes the Print External Notes and Print Internal Notes options are used in conjunction with other note-printing options. If you do not select at least one of these options for note-printing options that require them, no notes print, no matter what other options you select. At the same time, if you have one or both of these options selected, but you do not also have another option selected, no notes print.

For example, suppose you are printing a report that allows you to print both customer notes and customer order notes, and you can elect to print internal notes, external notes, or both. Suppose you want to print only external customer notes on the report. In this case, you would select Print Customer Notes (but not Print Order Notes) and Print External Notes (but not Print Internal Notes. If you do not select both options (Print Customer Notes and Print Internal Notes), no notes are printed.

On forms where Print External Notes and Print Internal Notes are the only 'print notes' options, it depends on the form itself as to which notes the system prints. For details about a specific form, see "Other Internal/External Notes Sources" in Printable Notes.

User notes and class notes do not print on reports.


Related Topics

About Forms, Fields, Records, and Collections

Reports Overview

Creating and Attaching Notes

Deleting Notes

Detaching Notes and Files

Reading and Modifying Notes

Class Notes

Object Notes

System/User Notes