When you print a report, the report data is first sent to the report generator and then to the printer. The system uses printing options as set on the Report Options form or the Intranets form. You have the option to select a printer other than your default printer. You can also preview the report before you actually print it.
To print a report:
Make sure the Output Format field for this report is set to Printer.
If no option record exists for your report, the report output defaults to the format as set on the Intranets form. The default output format on the Intranets form is Acrobat Format (PDF).
Click Select Printer.
The system opens the Report Options form.
In the Report Options form, if necessary, scroll to the right to locate the Printer Name column.
Specify the printer you want from the drop-down list.
Save and close the Report Options form.
You can select different printers for successive print jobs, but you must be careful: TaskMan uses whatever printer you have designated at the time it runs the print job.
Suppose, for example, that you queue up one print job to use Printer A and then a second print job to use Printer B. If TaskMan already had a queue and did not pick up the first job before you switched printers for the second job, then TaskMan uses Printer B for both print jobs.
To be safe, it is best to let one print job finish, if possible, before initiating the second print job.
For more information, see Previewing Reports.