E-Mailing Reports

When you send the report as an e-mail, the system sends it to the e-mail address entered on the Report Options form, or the Intranets form (if none is used on the Report Options form).

For more information about sending reports as e-mails to customers and vendors, see Sending Reports to Customers or Vendors.

To e-mail a report:

NOTE: Before reports can be printed, TaskMan must be set up as described in the System Administration Guide.
  1. (Optional) Verify that the Report Options form has been set up for the report you are running:
  2. Open the report form and define the report parameters.
  3. If the report is to be e-mailed to a customer or vendor, verify that:
  4. (Optional) Preview the report output. For more information, see Previewing Reports.
  5. Click Print.

Related Topics

Reports Overview

Report Options

Sending E-mail Notification

Faxing Reports

Intranets

Previewing Reports

Printing Reports