Many utilities, reports, and some activities can be scheduled to run daily, weekly, or monthly. Once scheduled, the process runs automatically in the background at a set time, using your selection criteria and option settings.
NOTE: Forms that can be scheduled to run in the background have the command Background in the Actions menu.
To run the process periodically, select Occurs every and specify an interval (for example, specify 24 Hours to run a process once a day) and a starting time.
To run a task one time only:
To schedule a task to run on a daily, weekly, or monthly basis, select that option from the left side. Then specify the occurrence information on the right side.
You can see which tasks are currently running by opening the Active Background Tasks form.
The task name should be the same as the report or utility's form name. If the task's status is WAITING, it is waiting for its scheduling requirements to occur. You can delete a WAITING task from the list.
Once the task has run, even if it fails, you can view details about its execution on the Background Task History form. Details include:
Scheduling Background Tasks (Developer or Administrator)
Setting Up Incremental Date Ranges for Reports That Run in the Background
Using Utilities and Activities