To view the elements and attributes of an IDO:
Open the IDOs form.
In the grid view, select the IDO you want to view.
When viewing the elements and attributes of an IDO keep these particulars in mind:
| This field or group of fields: | Does or tells you this: | ||
Attributes group |
The basic and identifying attributes for the IDO, which include:
For more information about specific attributes and elements in this group, use the context-sensitive help for the specific attribute or element (Right-click > Help). |
||
Group for source control status |
Revision status and check-out status of the IDO |
||
Buttons for modifications |
The row of buttons allow you to access a number of different forms from which you can gain additional information about elements of the IDO, add elements to the IDO, and make other modifications to the IDO. |
||
| This button: | Opens this form: | Which allows you to: | |
Tables |
View, add, and edit tables in the IDO |
||
Properties |
View, add, and edit properties for a designated table in the IDO |
||
Methods |
View, specify, and edit methods and stored procedures used within an IDO |
||
Filters |
View, specify, and edit criteria by which the data from the IDO collection is filtered |
||
New IDO |
Add an IDO to the associated IDO project |
||
New Table |
|
||
New Property |
Add a property to a designated table |
||
New Method |
Define a new method to be used with the IDO |
||
Status subcollection notebook |
In summary form, the elements and rules associated with the selected IDO: |
||
| This tab: | Displays a list and condensed view of: | ||
Tables |
All the tables associated with the IDO |
||
Properties |
All the properties defined in the IDO |
||
Methods |
All the methods associated with the IDO |
||
Filters |
The filters applied to the IDO, whether active or not |
||
Rules |
The rules that define relationships between IDOs and the policies to enforce when records are deleted |
||