Adding or Updating Information About a Unit Manually

You can add or update unit information automatically through utilities or through selections on the Service Parameters form. This topic describes how to add or update a unit manually through the Units form.

On the Units form, specify this information to describe a specific unit:

  1. In the header section, provide general information about the unit:

    Unit

    Specify the unit ID.

    Item

    Select an item number from those defined on the Items form.

    Customer Item

    Optionally, select a customer item.

    Description

    The item description is displayed from the Items form but can be overwritten.

    Customer

    Select the customer associated with the unit.

    Ship To

    The customer ship to location is displayed.

    Unit Status Code

    Select a status code to indicate the condition of the unit. These are maintained on the Unit Status Codes form.

    Last Meter Amount

    For new units, the last meter amount is set to zero. For existing units, the last meter reading amount is displayed.

    Last Meter Date

    For new units, the current date is displayed. For existing units, the last meter reading date is displayed.

    Warranty

    This field indicates whether any active warranty records exist for this unit. Warranty records are added to a unit or sub-component on the Unit Configurations form. An active warranty record has a starting date prior to the current date, and either no end date or one in the future.

    Originating Site

    Specify the location where the unit was originally built, if your system is multi-site.

  2. In the General tab, specify this information:

    Preventative Maint, Calibration, and Inspection

    Specify the last date that this type of work was done on the unit, and the next date that this type of work is scheduled to be performed on the unit.

    Full List Price and Sale Amount

    Specify the list price of the unit, and the price actually paid for this unit.

    Service Partner

    Specify the preferred partner to use for performing service on this unit.

    Priority Code

    Select a default priority code to use when this unit is added to an incident. For more information, see About Incident Escalation.

    Warehouse and Location

    Specify the warehouse and location of the unit.

    Available for Rental/Service

    Select these fields to indicate that the unit is available for rental or service. This field is informational only.

    Hold and Reason

    Select this field if the unit is currently on hold; that is, no maintenance is to be performed on the unit until the field is cleared. Then specify the reason for the hold.

    Install Date

    Specify the install date for the configuration. The value defaults to the current date but can be overwritten. This date is used by the As of Date calculation to determine what components are displayed.

    Ship Date

    Specify the date that the unit is shipped. If the Create Unit On Shipment field is selected in the Service Parameters form, this date is automatically updated to the shipment date when the unit is created during shipping.

    Manufacturer

    Specify the name of the manufacturer of the unit.

    Mfg #

    Specify the number assigned to the unit by the manufacturer.

    Region

    Specify the region that the unit is assigned to, as defined on the Service Regions form. On incidents or service orders where a unit is selected, the Region field defaults to the value specified here.

  3. In the Customer tab, specify the customer and consumer that currently owns or has possession of the unit. You can also record information about the original sales order to the customer.
  4. In the Maintenance tab, specify this information:

    Asset Number

    If the maintenance involves a fixed asset, select the number.

    Work Center

    Select the work center where the maintenance is performed.

    Resource

    Select the resource upon which the maintenance is performed.

    Copy Maint Button

    Click this button to copy the item planned maintenance schedule to use for the unit maintenance schedule.

    Active

    Select this check box if the maintenance line is currently active.

    SRO Type

    Select the SRO type.

    Frequency

    Select the frequency of the production of the service order:

    Month/Day

    These fields are enabled when the maintenance frequency is set to annual. Specify the month and day for the service.

    Date Duration

    Specify the length of time the maintenance requires. This value is used in conjunction with the Increment field to determine the calculation. This field is disabled when the frequency is set to annual.

    Increment

    Specify an increment for the service order. This field is disabled when the frequency is set to annual.

    Lead Time

    Specify length of time is needed in order to prepare for the work to be performed on a maintenance SRO.

    Increment

    Select a value that to use in conjunction with the Lead Time field for determining when the maintenance service order is created. Available options are:

    Start Date

    Select a date for the beginning of maintenance.

    Meter Amount

    The amount of miles, impressions, clicks, and so on that have been recorded for a specific unit is displayed. This value may be used to determine if a unit is currently under warranty.

    SRO

    Select the SRO.

    SRO Line

    Select the SRO line.

    Last SRO Num

    The last service order that was generated for the maintenance line is displayed.

    Shift ID

    Select a valid shift. The resource will be available for work during the intervals specified on this shift. You can set up shift intervals on the Scheduling Shifts form.

    Start Time

    Specify the start time for the current record.

    Down Time

    Specify the number of days needed to perform maintenance work. This information is used with scheduling equipment in a plant maintenance scenario to ensure that work is not performed while the equipment is unavailable.

    Schedule Basis

    Select whether maintenance service orders are generated based on the end date, close date, or maintenance date of the last SRO.

    Schedule Future

    Select this check box to create maintenance service orders based on the frequency selected and regardless of any prior SROs that are open in the system for the selected maintenance line.

  5. Use the Service History tab to view information about the unit's service history. Select a record and click View to display the Service Order Lines form for that record.
  6. Use the Incidents tab to view information about incidents involving this unit. Select a record and click View to display the Incidents form for that record.
  7. Use the Owner History tab to view information about the owner of the unit.
  8. Use the Status History tab to track updates that were added for the unit status code. Records can be appended either manually through the Units form or remotely through the Service Management Mobile module. By default, the grid records are sorted by date column, with the most recent record at the top of the list.

    Date

    The date and time of the unit status change are displayed.

    Status

    The unit status code is displayed.

    Partner

    The partner who performed the unit status change is displayed.

    Source Type

    The source of the unit status update is displayed. Options are SRO, Incident, and Unit.

    Source

    For the unit source type, this field is blank.

  9. Use the Meter History tab to track updates that were made to the unit meter amount. Records can be added to this grid in several ways: manually on this tab, through triggers on the meter amount field on the Incidents, Service Order Lines, and Units form, or remotely from the Service Management Mobile application.

    By default, the grid records are sorted by date column, with the most recent record at the top of the list.

    Date

    The date that the meter amount was recorded is displayed.

    Meter Reading

    The amount of miles, impressions, clicks, and so on that have been recorded for a specific unit is displayed. This value may be used to determine if a unit is currently under warranty.

    Partner

    The partner who performs the meter reading and enters the updated amount is displayed.

    Source Type

    The source of the meter update is displayed. Options are SRO, incident, or unit.

    Source

    For the unit source type, this field is blank.

  10. Save the record.

Other Ways to Use the Units Form

Use these buttons on the form as described here:


Related Topics

Setting Up the System for Units

About Items, Units and Servicing