Reconciling Partner Expenses

Use the Expense Reconciliation form and Expense Reconciliation Process modal form to reconcile partner expenses.

To reconcile expenses:

  1. On the Expense Reconciliation form, specify this information:

    Payment Type

    Select the code for the payment type being used. The available selections are set up and maintained using the Payment Types form.

    Description

    A description of the payment type is displayed.

    Unreconciled Only

    Select this check box to display only expenses that are not reconciled.

    Approved Only

    Select this check box to display only expenses that have been approved.

    Miscellaneous Charges

    Specify any additional miscellaneous charges to include in the process.

    Selected

    The running total of expenses selected for reimbursement is displayed.

    Total

    The subtotal of reimbursements due, based on the additional charges and Selected field is displayed.

    Amount Due

    Specify the total amount of expense reimbursement that is due.

  2. Click Voucher to launch the Expense Reconciliation Process modal form, filtered for the selected payment type.

  3. Select the vendor for whom you are creating the voucher.

  4. Specify the vendor invoice number to be written on the voucher.

  5. Click Process to complete the expense reconciliation.

To stop the process, click Cancel.

Buttons

Click Clear to launch the Expense Reconciliation Process modal form and clear the charges.

Click Select All to mark all records for processing.

Click Deselect All to remove the selected records for processing.


Related Topics

Approving Partner Expenses

Reimbursing Partner Expenses