Customer Order Blanket Releases

Use this form to add releases to blanket lines on a blanket order. A blanket order ships items to a customer in a staggered manner.

By adding releases to individual lines, you determine the ship dates of the items. A blanket order can have multiple lines, or multiple items. A blanket line can have multiple releases, or multiple ship dates.

In the EU VAT tab, the fields are used by the European Union (EU). If the Activate EU VAT Reporting field on the General Parameters form is not selected, this tab (or some fields on this tab) are disabled.

Actions Menu

The Actions menu includes the option Go to Demand Detail Chart APS, which opens the Demand Detail Chart APS form. This option displays a graphical representation of how the system uses supplies, on-hand inventory, and resource capacity to satisfy the demand at each level of the bill of material.

The Actions menu also includes options to filter the data to show only lines where the due date is 7, 14 or 30 days in the future, and an option to show only lines where the due date is any number of days past due.


Related Topics

Customer Orders Overview

Configuring an Item from a Customer Order Line (Regular or Blanket)

Creating a Blanket Order

Using Demand and Source Vendor Site PO-CO Automation

About Credit Hold

About Cross-Referenced Blanket Releases and Order Shipping

About DIFOT (Delivered In Full and On Time)

Customer Order Blanket Lines

Customer Orders