Customer Order Lines

The customer order line/release is a detailed listing associated with the customer order header record, which describes any item sold to a customer. Multiple lines/releases may be associated with a customer order header.

Customer Order Lines and Credit Hold

If this customer is on credit hold, a problem indicator is displayed at the top of the form. If this customer is not on credit hold, a check mark is displayed.

You cannot cross-reference a customer order line if the customer order is on credit hold. However, if the customer order line is cross-referenced before the customer order is placed on credit hold, the reference information is maintained.

If either the Customer Order Credit Hold field or the Customer Credit Hold field is selected, the system does not let you ship customer orders.

If the Limit Exceeded Credit Hold Reason field, however, is blank, and you create or update a customer order or a customer order line when the customer's (or corporate customer's, if applicable) credit limit is exceeded, the system does not place the customer order on credit hold and does not prevent you from shipping the order.

In the EU VAT tab, the fields are used by the European Union (EU). If the Activate EU Reporting field on the General Parameters form is not selected, this tab (or some fields on this tab) is disabled.

About Unit Prices

When a line/release item quantity is changed and saved, the Unit Price field is not updated to reflect any change to the unit price in the Items form.

EXAMPLE: On June 15, a customer orders five items at $20.00/item. On June 16, the Items Unit Price changes to $22.00. If on June 17, the CO is updated to six items, the items remain priced at $20.00/item (according to the CO).

If the Qty Ordered field is changed, the Allocated to Customer Orders field on the Items form is adjusted.

Actions Menu

The Actions menu includes these options:


Related Topics

Customer Orders Overview

Order Entry Steps

About Customer Order Entry for Non-Inventory Items

Adding a Configured Item in Order Entry

Configuring a Customer Order

Configuring an Item from a Customer Order Line (Regular or Blanket)

Changing Lines/Releases to a Status of Complete

Creating a Customer Contract

Cross-Referencing Demands to Supplies

Defining and Processing a Kit

Reserving Inventory for an Order

Using Demand and Source Vendor Site PO-CO Automation

About Credit Hold

Using Credit Hold

About Incremental Planning and ATP/CTP

About DIFOT (Delivered In Full and On Time)

About Drop-Ship Locations and Taxes on Customer Order Lines

Determining the Best Site/Warehouse to Fulfill an Order

European Union (EU) Supplemental Information