Order Entry Steps
To create, ship, and invoice a customer order:
	- Enter a new customer order on the Customer 
	 Orders form.
- Enter the appropriate information in all required 
	 fields. 
- Save the customer order.
- To open the Customer 
	 Order Lines form, click the Lines button.
- Add order lines and/or releases to the order. 
	
		NOTES: 
		
			- Alternatively, you can quickly create an entire customer 
			 order on the Customer 
			 Orders Quick Entry form.
- The system displays warning messages if you add an item 
			 flagged obsolete 
			 or slow-moving to a customer order.
- If you will be cross-referencing the customer order line 
			 to a job or purchase order, see Cross-Referencing 
			 Demands to Supplies for the steps.
- If you need to check availability of the item before completing 
			 the order, click Get ATP or Get CTP and see 
			 the Help topic for the Availability 
			 Results form for details about the information that 
			 displays.
 
 
- Save the customer order line. If the Allow Over Credit Limit field 
	 is selected, the record is saved as-is. If the Allow Over Credit Limit 
	 field is not selected,  the system checks if the order total 
	 is less than, or equal to, the total available credit for the customer. 
	 If it is, the system then checks if the order total is less than, 
	 or equal to, the order credit limit, if specified. If it is, the record 
	 is saved. If the order fails these checks, the order status is changed 
	 to Planned, a warning message displays, and the record is saved.
- If the order has a long lead time and your customer requires a 
	 hard-copy order acknowledgement, print the Order 
	 Verification Report.
- Ship the order. 
	For the steps, see Shipping 
	 Customer Orders. You can print the packing list before or after 
	 shipping transactions. 
- Invoice the order. 
	For the steps, see Invoicing 
	 a Customer Order. When you print the invoice, the system also 
	 posts the record to Accounts Receivable. For more information, see 
	 Accounts 
	 Receivable Steps. 
Related Topics
Changing 
 Lines/Releases to a Status of Complete
Changing 
 Order Status to History
Configuring 
 a Customer Order
Creating a 
 Blanket Order
Creating a Customer
Creating 
 a Customer Contract
Customer 
 Orders and Invoices in Foreign Currencies
Deleting 
 a Customer Order
Generating 
 a Progressive Billing - Method 1
Generating 
 a Progressive Billing - Method 2
Performing 
 a Quick Return of an Entire Order
Printing 
 a Progressive Bill
Setting 
 Up Customer Order Entry
Shipping 
 Customer Orders
Customer 
 Orders Quick Entry