Use this form to record how the items will be packed for a shipment. You can also use it to move inventory assigned to a shipment from the packing location to the shipping (or staging) location. Packages are not required to be created for shipments and the inventory can remain at the packing location. For more information, see Pack Confirmation Scenarios.
If multiple item lines are selected, all of the picked quantities for all selected lines are moved into one package, whether it is a serial item or not.
This grid contains an Items tab and a Serial Numbers tab. The Items tab is used to select which items and what quantity should be put into packages. The Serial Numbers tab is used to select which serial numbers should be put into packages. Other than the select check box, both tabs are read-only.
The packages grid displays the packages that were created by the use of the Create/Add To Packages button. The following fields display in this grid:
This grid contains an Items tab and a Serial Numbers tab. Both tabs are read-only and their grids are populated when you select a package in the packages grid.