Calculating Unit Price for Customer Orders/Estimates

Unit price is calculated as:

Unit Price = Base + or (-) Dollar Amount or Percent

The system performs several actions when determining the Unit Price on Customer Orders, EDI Customer Orders, Customer Order Lines, or Estimate Lines:

  1. Checks to see if a promotion pricing code has been specified for the selected customer order line. If there is no promotion pricing for the order line, the system moves on to step 2.
  2. Checks to see if a Customer Contracts record is set up for that customer, item, and customer-item combination. If a record with this combination is not found, then it looks for a record with a matching customer and item, and a null customer-item. If one of these types of records is found, then the system checks the customer-item pricing table to find a record where the order due date is on or after the effective date. If a valid pricing record is found, and the contract price has a value, it uses that contract price. If the contract price is zero, the system moves on to step 3.
  3. Determines if any quantity price breaks have been established for the customer and item by checking the Customer Contracts Prices record. If quantity price breaks exist, they will be used as the default Unit Price. If there are no quantity price breaks for the customer, the system moves on to step 4.
  4. Determines whether a customer price code is available for the customer order line release or EDI customer order line release as well as an item price code from the item pricing record. If either price code is not found, the system moves on to step 5. If both price codes are available, the system uses the Price Matrix Table to determine the price. After the system determines that two valid price codes exist, it searches the Price Matrix Table to determine if a price code record exists for this combination of codes.

    If the system locates a Price Matrix record, the corresponding Price Formula is used in calculating the item's Unit price. The system then cross checks the quantity price breaks:

  5. Searches for a current Item Pricing record based on the item pricing's effective date and customer's currency code.
  6. If no Item Pricing record exists, a message displays, stating that not one item price exists. In this case, you must enter the price manually.

NOTES:


Related Topics

Calculating Unit Price for Inter-Entity Transfer Orders

Customer Contracts Pricing Setup

Setting Up Customer Contracts for Contract Manufacturing

Promotion Pricing and Rebate Programs Overview