Shipping schedules that are received reflect the new quantities the customer is expecting, less any quantities from advance ship notices imported into the translator. (Customers may at anytime increase or decrease the quantity ordered.) All SyteLine customer order releases must be deleted and replaced with the new releases and quantities. Release processing for 830/862 EDI transactions uses "Replace Logic."
Replace logic deletes any SyteLine releases with 0 shipped quantities and updates any unfilled releases with a quantity shipped as "Filled." The new imported releases, less any shipped quantities on ASN not exported to the translator, are added to the SyteLine customer order.
The EDI Customer Profile form contains three fields which define replacement logic processing:
The following examples help to illustrate what happens with different settings of these fields:
The system assumes the incoming flat file accurately reflects the new requirements and will post the incoming requirements to the customer order exactly as they are.
The incoming 830/862 has the following release requirements for a single item.
| Releases | Due Date | Qty Required |
|---|---|---|
| 1 | 8/7 | 336 |
| 2 | 8/9 | 336 |
| 3 | 8/10 | 336 |
| 4 | 8/13 | 504 |
| 5 | 8/14 | 336 |
| 6 | 8/15 | 336 |
Scenario # 1:
Import the above requirements. The customer order will reflect releases 1 thru 6 for this particular line. Ship releases 1 and 2, then re-import the same requirements as shown above. The customer order will reflect 8 releases as shown in the following table:
| Releases | Due Date | Released | Shipped | Status |
|---|---|---|---|---|
| 1 | 8/7 | 336 | 336 | F |
| 2 | 8/9 | 336 | 336 | F |
| 3 | 8/7 | 336 | O | |
| 4 | 8/9 | 336 | O | |
| 5 | 8/10 | 336 | O | |
| 6 | 8/13 | 504 | O | |
| 7 | 8/14 | 336 | O | |
| 8 | 8/15 | 336 | O |
Scenario #2:
Assume the original 6 releases have been imported and posted to the customer order. Ship the total quantity for release 1 (336) but only ship 100 against release 2. Then re-import the same 6 releases and post. The customer order will show 8 releases as follows:
| Releases | Due Date | Released | Shipped | Status |
|---|---|---|---|---|
| 1 | 8/7 | 336 | 336 | F |
| 2 | 8/9 | 336 | 100 | F |
| 3 | 8/7 | 336 | O | |
| 4 | 8/9 | 336 | O | |
| 5 | 8/10 | 336 | O | |
| 6 | 8/13 | 504 | O | |
| 7 | 8/14 | 336 | O | |
| 8 | 8/15 | 336 | O |
Scenario # 3:
Assume the original 6 releases have been imported and posted against the customer order. Ship a quantity of 400 against release 1. Re-import the original 6 releases and post. The customer order will now have 7 releases as follows:
| Releases | Due Date | Released | Shipped | Status |
|---|---|---|---|---|
| 1 | 8/7 | 336 | 400 | F |
| 2 | 8/7 | 336 | O | |
| 3 | 8/9 | 336 | O | |
| 4 | 8/10 | 336 | O | |
| 5 | 8/13 | 504 | O | |
| 6 | 8/14 | 336 | O | |
| 7 | 8/15 | 336 | O |
Summary: If you do not activate the Generate Ship Notice option in the EDI Customer Profile, the incoming flat file must reflect the current customer requirements and will not take any prior requirements or changes into consideration when posting the incoming releases.
The system will replace the current line releases with the incoming requirements but will take into account prior shipments made.
The incoming 830/862 flat file has the following release requirements for a single item.
| Releases | Due Date | Qty Required |
|---|---|---|
| 1 | 8/7 | 336 |
| 2 | 8/9 | 336 |
| 3 | 8/10 | 336 |
| 4 | 8/13 | 504 |
| 5 | 8/14 | 336 |
| 6 | 8/15 | 336 |
Scenario #1:
Import the above requirements. The customer order will reflect releases 1 thru 6 for this particular line. Ship release 1, then re-import the same requirements as shown above. The customer order will reflect 6 releases as follows:
| Releases | Due Date | Released | Shipped | Status |
|---|---|---|---|---|
| 1 | 8/7 | 336 | 336 | F |
| 2 | 8/9 | 336 | O | |
| 3 | 8/10 | 336 | O | |
| 4 | 8/13 | 504 | O | |
| 5 | 8/14 | 336 | O | |
| 6 | 8/15 | 336 | O |
Scenario #2:
Import the original flat file to a new order. Ship 336 against release 2. Re-import the original flat file and the customer order will reflect 6 releases as follows:
| Releases | Due Date | Released | Shipped | Status |
|---|---|---|---|---|
| 2 | 8/9 | 336 | 336 | F |
| 3 | 8/7 | 336 | O | |
| 4 | 8/10 | 336 | O | |
| 5 | 8/13 | 504 | O | |
| 6 | 8/14 | 336 | O | |
| 7 | 8/15 | 336 | O |
Scenario #3:
Assume the original 6 releases have been imported and posted to a new customer order. Ship 336 against release 1 and 100 against release 2. Re-import the original 6 releases and post. The customer order will show 7 releases as follows:
| Releases | Due Date | Released | Shipped | Status |
|---|---|---|---|---|
| 1 | 8/7 | 336 | 336 | F |
| 2 | 8/9 | 336 | 100 | F |
| 3 | 8/9 | 236 | O | |
| 4 | 8/10 | 336 | O | |
| 5 | 8/13 | 504 | O | |
| 6 | 8/14 | 336 | O | |
| 7 | 8/15 | 336 | O |
Scenario #4:
The original 6 releases have been imported and posted creating a new customer order. Ship 500 against release 1. Re-import the original 6 releases and post to the customer order. The customer order will now show 6 releases as follows:
| Releases | Due Date | Released | Shipped | Status |
|---|---|---|---|---|
| 1 | 8/7 | 336 | 500 | F |
| 2 | 8/9 | 172 | O | |
| 3 | 8/10 | 336 | O | |
| 4 | 8/13 | 504 | O | |
| 5 | 8/14 | 336 | O | |
| 6 | 8/15 | 336 | O |
Scenario #5:
If you have an EDI order that you have been receiving requirements against when the EDI Customer Profile did not have the Generate Ship Notice check box selected, and then you turn on the generate ASN's the system will look at the shipments against the line to day and reduce the incoming Requirements by the quantities shipped. Using the same situation from Scenario #1, import the original file with the Generate Ship Notice check box cleared. Then ship releases 1 and 2 and import the same file again. The customer order will have 8 releases. Activate the ASN in the EDI Customer Profile and import the original 6 releases again. The posted customer order will show the following releases:
| Releases | Due Date | Released | Shipped | Status |
|---|---|---|---|---|
| 1 | 8/7 | 336 | 336 | F |
| 2 | 8/9 | 336 | 336 | F |
| 3 | 8/10 | 336 | O | |
| 4 | 8/13 | 504 | O | |
| 5 | 8/14 | 336 | O | |
| 6 | 8/15 | 336 | O |
In this case, the customer order had 8 releases and after turning on the generate ASN's and importing the same requirements again, the system replaced the 8 releases with the incoming requirements less quantities shipped to show the total requirements based on the last import. If releases 1 and 2 had not been on the new import, then the system would have adjusted releases 3 and 4 for the shipments previously made against this order.
NOTE: If you are using a translator with CUM capabilities, such as Radley's CARaS, you must export the ASNs prior to importing the 830/862s so that CARaS can adjust the incoming requirements appropriately.
In the previous examples we imported the same 830\862 requirements each time as a second import without generating and exporting ASN documents. These examples show what happens if the ASN document has been exported for shipments made.
The incoming 830/862 has the following release requirements for a single item.
| Releases | Due Date | Qty Required |
|---|---|---|
| 1 | 8/7 | 336 |
| 2 | 8/9 | 336 |
| 3 | 8/10 | 336 |
| 4 | 8/13 | 504 |
| 5 | 8/14 | 336 |
| 6 | 8/15 | 336 |
Scenario #1:
Import the above requirements. The customer order will reflect releases 1 thru 6 for this particular line. Ship releases 1, Generate and export the ASN for shipment. Then re-import the same requirements as shown above. The customer order will reflect 7 releases as follows:
| Releases | Due Date | Released | Shipped | Status |
|---|---|---|---|---|
| 1 | 8/7 | 336 | 336 | F |
| 2 | 8/7 | 336 | O | |
| 3 | 8/9 | 336 | O | |
| 4 | 8/10 | 336 | O | |
| 5 | 8/13 | 504 | O | |
| 6 | 8/14 | 336 | O | |
| 7 | 8/15 | 336 | O |
Scenario #2:
Assume the original 6 releases have been imported and posted to a new customer order. Ship 336 against release 1 and 100 against release 2. Generate and export the ASN. Re-import the original 6 releases and post. The customer order will show 8 releases as follows:
| Releases | Due Date | Released | Shipped | Status |
|---|---|---|---|---|
| 1 | 8/7 | 336 | 336 | F |
| 2 | 8/9 | 336 | 100 | F |
| 3 | 8/7 | 336 | O | |
| 4 | 8/9 | 336 | O | |
| 5 | 8/10 | 336 | O | |
| 6 | 8/13 | 504 | O | |
| 7 | 8/14 | 336 | O | |
| 8 | 8/15 | 336 | O |
Scenario #3:
Assume the original 6 releases have been imported and posted to a new customer order. Ship 336 against release 1. Generate and export the ASN. Then ship 100 against release 2 but do not generate and export the ASN. Re-import the original 6 releases and post. The customer order will show 8 releases as follows:
| Releases | Due Date | Released | Shipped | Status |
|---|---|---|---|---|
| 1 | 8/7 | 336 | 336 | F |
| 2 | 8/9 | 336 | 100 | F |
| 3 | 8/7 | 236 | O | |
| 4 | 8/9 | 336 | O | |
| 5 | 8/10 | 336 | O | |
| 6 | 8/13 | 504 | O | |
| 7 | 8/14 | 336 | O | |
| 8 | 8/15 | 336 | O |
Because the 100 pieces shipped on release 2 were not exported to the trading partner they are deducted from the incoming releases on the second import.
In the previous examples we imported the same 830\862 requirements each time as a second import. This example shows what happens with replacement logic when different releases in the 830\862 file are being imported the second time.
Assume we import the same 830\862 release first time as before.
| Releases | Due Date | Qty Required |
|---|---|---|
| 1 | 8/7 | 336 |
| 2 | 8/9 | 336 |
| 3 | 8/10 | 336 |
| 4 | 8/13 | 504 |
| 5 | 8/14 | 336 |
| 6 | 8/15 | 336 |
We then ship 336 pieces on the 8/7 and 8/9 releases. We do not generate and export the ASN.
Then we import a new 830\862 with following releases:
| Releases | Due Date | Qty Required |
|---|---|---|
| 1 | 8/10 | 336 |
| 2 | 8/11 | 336 |
| 3 | 8/12 | 336 |
| 4 | 8/13 | 504 |
| 5 | 8/14 | 336 |
| 6 | 8/15 | 336 |
The customer order will show 6 releases as follows:
| Releases | Due Date | Released | Shipped | Status |
|---|---|---|---|---|
| 1 | 8/7 | 336 | 336 | F |
| 2 | 8/9 | 336 | 336 | F |
| 3 | 8/12 | 336 | O | |
| 4 | 8/13 | 504 | O | |
| 5 | 8/14 | 336 | O | |
| 6 | 8/15 | 336 | O |
Although this example appears to have dropped the requirements for 8/10 and 8/11 this is correct since the ASN was not exported. The system deducts the two shipments of 336 each from the new incoming 830/862 releases because the trading partner was not aware of the shipments.
In the previous example we imported 830\862 document with changed requirements as second import. This example shows what happens with replacement logic when a different releases are in the 830\862 file being imported the second time and ASN has been generated and exported.
Assume we import the same 830\862 release first time as before.
| Releases | Due Date | Qty Required |
|---|---|---|
| 1 | 8/7 | 336 |
| 2 | 8/9 | 336 |
| 3 | 8/10 | 336 |
| 4 | 8/13 | 504 |
| 5 | 8/14 | 336 |
| 6 | 8/15 | 336 |
We then ship 336 pieces on the 8/7 and 8/9 releases. This time we generate and export the ASN. Then we import a new 830\862 with following releases:
| Releases | Due Date | Qty Required |
|---|---|---|
| 1 | 8/10 | 336 |
| 2 | 8/11 | 336 |
| 3 | 8/12 | 336 |
| 4 | 8/13 | 504 |
| 5 | 8/14 | 336 |
| 6 | 8/15 | 336 |
The customer order will show 8 releases as follows:
| Releases | Due Date | Released | Shipped | Status |
|---|---|---|---|---|
| 1 | 8/7 | 336 | 336 | F |
| 2 | 8/9 | 336 | 336 | F |
| 3 | 8/10 | 336 | O | |
| 4 | 8/11 | 336 | O | |
| 5 | 8/12 | 336 | O | |
| 6 | 8/13 | 504 | O | |
| 7 | 8/14 | 336 | O | |
| 8 | 8/15 | 336 | O |
This example shows the effect on releases due to the Replace Planning Schedules setting.
Assume we import an 830\862 release as follows.
| Releases | Due Date | Qty Required | Status |
|---|---|---|---|
| 1 | 8/7 | 336 | O |
| 2 | 8/9 | 336 | O |
| 3 | 8/10 | 336 | O |
| 4 | 8/13 | 504 | O |
| 5 | 8/14 | 336 | O |
| 6 | 8/15 | 336 | O |
| 7 | 9/30 | 336 | P |
| 8 | 10/30 | 336 | P |
| 9 | 11/30 | 336 | P |
| 10 | 12/30 | 336 | P |
We then ship 336 pieces on the 8/7 and 8/9 releases. This time we generate and export the ASN.
Then we import a new 830\862 with following releases:
| Releases | Due Date | Qty Required | Status |
|---|---|---|---|
| 1 | 8/7 | 336 | O |
| 2 | 8/9 | 336 | O |
| 3 | 8/10 | 336 | O |
| 4 | 8/13 | 504 | O |
| 5 | 8/14 | 336 | O |
| 6 | 8/15 | 336 | O |
| 7 | 9/30 | 336 | P |
| 8 | 10/30 | 336 | P |
| 9 | 11/30 | 336 | P |
The customer order will show 10 releases as follows:
| Releases | Due Date | Released | Shipped | Status |
|---|---|---|---|---|
| 1 | 8/7 | 336 | 336 | F |
| 2 | 8/9 | 336 | 336 | F |
| 3 | 8/10 | 336 | O | |
| 4 | 8/13 | 336 | O | |
| 5 | 8/14 | 336 | O | |
| 6 | 8/15 | 504 | O | |
| 7 | 9/30 | 336 | P | |
| 8 | 10/30 | 336 | P | |
| 9 | 11/30 | 336 | P | |
| 10 | 12/30 | 336 | P |
This is because of the replace planning schedule flag is not checked so releases with later dates than the incoming 830\862 planning schedules are retained.
Assume we import an 830\862 release as follows.
| Releases | Due Date | Qty Required | Status |
|---|---|---|---|
| 1 | 8/7 | 336 | O |
| 2 | 8/9 | 336 | O |
| 3 | 8/10 | 336 | O |
| 4 | 8/13 | 504 | O |
| 5 | 8/14 | 336 | O |
| 6 | 8/15 | 336 | O |
| 7 | 9/30 | 336 | P |
| 8 | 10/30 | 336 | P |
| 9 | 11/30 | 336 | P |
| 10 | 12/30 | 336 | P |
We then ship 336 pieces on the 8/7 and 8/9 releases. This time we generate and export the ASN.
Then we import a new 830\862 with following releases:
| Releases | Due Date | Qty Required | Status |
|---|---|---|---|
| 1 | 8/7 | 336 | O |
| 2 | 8/9 | 336 | O |
| 3 | 8/10 | 336 | O |
| 4 | 8/13 | 504 | O |
| 5 | 8/14 | 336 | O |
| 6 | 8/15 | 336 | O |
| 7 | 9/30 | 336 | P |
| 8 | 10/30 | 336 | P |
| 9 | 11/30 | 336 | P |
The customer order will show 9 releases as follows:
| Releases | Due Date | Released | Shipped | Status |
|---|---|---|---|---|
| 1 | 8/7 | 336 | 336 | F |
| 2 | 8/9 | 336 | 336 | F |
| 3 | 8/10 | 336 | O | |
| 4 | 8/13 | 336 | O | |
| 5 | 8/14 | 336 | O | |
| 6 | 8/15 | 504 | O | |
| 7 | 9/30 | 336 | P | |
| 8 | 10/30 | 336 | P | |
| 9 | 11/30 | 336 | P |
This is because the replace planning schedules flag is checked. Releases with dates later than the incoming 830\862 planning schedule are removed from the order.