Automatic Vouchering 
Normally, vouchers for material received are created using the Generate A/P 
 Transactions or Voucher 
 Builder forms.  However, you can avoid that step by setting 
 up your vendors to use automatic vouchering.  Follow these steps 
 to configure the system:
Configure Vendors
	- Open the Vendors form.
- For each vendor that will be participating in automatic vouchering, 
	 select the Auto 
	 Voucher field. All purchase orders created for these vendors 
	 will default to Auto Voucher.
- Select the Auto 
	 Voucher Method.
- Save the record.
Create/Modify Purchase Orders
When you create a purchase order, whether on the 
 Purchase Orders, 
 Purchase 
 Order Builder, or Purchase 
 Orders Quick Entry form, the Auto 
 Voucher field will default to the setting made at the vendor level. 
 Accept the default or change it.
Receiving Purchase Orders
	- Open the Purchase 
	 Order Receiving form.
- When you receive 
	 a purchase order line/release, several conditions are checked: 
	
		- Is the receipt positive (auto vouchering does not apply to 
		 negative receipts or debit returns)?
- Is a vendor assigned to this purchase order?
- Is the purchase order configured to autovoucher?
 
- If you are receiving lines from multiple POs, additional conditions 
	 must be met: 
	
		-  All POs must 
		 have the same value for the Include 
		 Tax in Costs field 
- All POs must have the same value for the Fixed 
		 Rate field, and if Fixed Rate is selected, then they must 
		 have the same exchange rate.  
- All POs must have the same value for Billing Terms. 
 
- When you click Receive, the system compiles a list of all lines/releases 
	 that meet the above conditions.
- If the vendor's Auto Voucher Method 
	 is Automatic, then the system 
	 automatically creates the voucher and a success message indicates 
	 the voucher number that was created.
- If the vendor's Auto Voucher Method 
	 is Prompt, then the Purchase 
	 Order Receiving Auto Voucher form opens. Accept the defaults, 
	 or enter new data, then click OK. 
	  A success message indicates the voucher number that was created. 
	 
	If you do not have permission to open this form, 
	 automatic vouchering will not occur at this time, regardless of the 
	 settings. 
- Click OK.  A confirmation 
	 message displays.
If the pre-existing 
 receipts have different costs, they are vouchered at the cost of the latest 
 receipt and an offsetting journal entry is created.
Related Topics
Purchasing Overview
Creating 
 a Voucher or Adjustment"