Creating Vouchers or Adjustments
There are two ways to automatically generate vouchers: configure the 
 Auto 
 Voucher feature for each vendor, or use the Generate 
 A/P Transactions form.  For 
 more information about using the Auto Voucher feature, see Automatic 
 Vouchering.  For more 
 information regarding the Generate 
 A/P Transactions form, continue 
 reading this topic.
To automatically create adjustments, 
 however, follow these steps using the Generate 
 A/P Transactions form:
	- Display receipts for purchase 
	 order lines.
- Edit the lines to reconcile receipts 
	 with the vendor's invoice.
- Create pending tax transaction 
	 lines for the received purchase orders.
- Enter payable amounts in the 
	 voucher header.
- Generate the voucher or adjustment.
Display 
 Receipts for Purchase Order Lines
	- Select the vendor whose invoice you are entering.
- Do one of the following: 
	
		- To create a voucher for received purchase order lines, select 
		 the Voucher option.
- To create an adjustment to an existing voucher for returned 
		 items, select the Adjustment option.
 
- If you selected the Adjustment option, in the Voucher 
	 field, select the existing voucher number.
- In the G/L Dist field, select a date or accept the default, 
	 which is the current date. The date is the record date of the accounts 
	 payable transaction.
- To link the new voucher to a voucher pre-register, select the voucher 
	 pre-register number, and then select OK. For details, see Pre-Register.
- Select the Additional Material Selection tab.
Vouchering Purchase Order Lines
	- Select the Generate from PO check box.
- Select the range of purchase orders you want to use.
- Select the lines/releases you want to use. 
	NOTE: If the 
	 unit of measure of a purchase order line item was changed to something 
	 other than the original unit of measure listed on the Items 
	 form, the Generate 
	 A/P Transactions utility uses the original unit of measure to 
	 validate the data. 
Vouchering GRN Lines
	- Select the Generate from GRN check box.
- Select the range of GRNs appearing in the invoice.
- (Optional) Select the range of GRN line numbers appearing in the 
	 vendor's invoice.
- (Optional) Select the range of purchase order numbers appearing 
	 in the vendor's invoice.
Vouchering EDI Invoices
Selecting the Generate from EDI Invoices check box clears any 
 values currently in the Generate from PO and Generate from GRN 
 fields of the Additional Material Selection tab and disables those 
 fields.
	- Select the Generate from EDI Invoices check box. This field 
	 is disabled if the vendor is not set up for EDI transactions or if 
	 there are any pending transactions currently on the Material 
	 tab or the Taxes tab.
- Select an invoice.
- To include GRN lines, select the Received via GRN check 
	 box and select a GRN number in the GRN field.
- Select Select Matching. Receipts for purchase order lines 
	 display in the browser on the Material tab.
Edit Receipts for 
 Purchase Order Lines
When you edit receipt lines, the amount in the Total field on 
 the Material tab is automatically recalculated.
	- Delete any purchase order receipt lines or GRN lines in the Material 
	 tab that are not referred to in the vendor's invoice.
- In the To Vch/Adj field, modify (as required) the number 
	 of units of each line item to include in the voucher, or accept the 
	 default value of the quantity received minus any quantity previously 
	 vouched for the purchase order line or GRN line.
- Modify (as required) the unit cost of each line, or accept the 
	 default value.
Create Tax Transaction 
 Lines
The Taxes tab is enabled when the Active for Purchasing 
 check box is selected on the Tax 
 Systems form for at least one tax system.
If the Taxes tab is disabled, you can enter tax amount(s) from 
 the vendor's invoice, or other amounts as required, in the Sales Tax 
 field(s) on the header.
	- Select the Taxes tab.
- Select Generate Tax. The activity calculates the sales tax 
	 for each pending voucher line on the Material tab and creates 
	 a pending tax transaction line for each purchase order on which tax 
	 is owed. The activity displays the total of the line amounts in the 
	 Sales Tax field(s) on the Taxes tab and provides the 
	 option of copying the sum(s) to the header. 
	NOTE: The label 
	 for the Sales Tax field is user-defined. 
- To add a tax amount that was not created in the generation process, 
	 create a new tax transaction line.
Enter Payable Amounts 
 in the Header
	- In the Material field on the header, enter the amount displayed 
	 in the Total field on the Material tab. Amounts in the 
	 two fields must be equal. The amount should be equal to what is specified 
	 on the vendor's invoice.
- In the Freight and Misc Charges fields on the header, 
	 enter amounts from the vendor's invoice or as required.
- If you have not already entered sales tax on the header, do so 
	 now. Sales Tax amount(s) on the header must equal the total(s) 
	 on the Taxes tab.
- If you are creating a non-EDI voucher or adjustment, select the 
	 General tab and enter the required information.
Generate the Voucher
Select Generate.
The new voucher number appears in a message when processing is complete.
Related Topics
Purchasing 
 Overview
Creating 
 Multi-Site Vouchers and Adjustments with the Voucher Builder
Creating 
 Vouchers or Adjustments Manually
Reversing 
 a Voucher Generated from Purchasing