Creating Estimate Lines

To add line items to an existing estimate, use the Estimate Lines form.

  1. In the Estimate field, select the estimate to which you want to add an estimate line item.
  2. Add a new line, entering the appropriate data in these required fields:
  3. (Optional) Set the following fields as desired:
  4. To either create or go to a cross-reference record, click Source.

    If the reference fields are blank, the system adds a new record, based on the reference type. After you create the new job or project, the system updates the estimate line to reflect the cross reference.

    NOTE: You can attach or cross reference this estimate line to a specific job or project. You cannot cross reference this estimate line to a transfer, purchase order or purchase requisition.

  5. Select Actions > Save.

NOTES: If the current estimate line is configured, you can see a listing of the configured options by selecting Actions > List Configuration Values.

Estimate lines can also be created by using the copy facility. For more information, see Copying Orders and Estimates.

When you source an estimate line to an estimate project and the customer on the estimate is blank and the estimate line's source is Project, then if you have at least one project type with non-billable pricing set up, the system uses the first of those project types as the default type, and creation of the estimate project can continue. It the customer on the estimate is not blank, the system uses the first project type with Fixed Price pricing. Otherwise, an error is displayed.

If you change an existing Estimate Line item, and the quantity is changed, you will receive a confirmation of the change and the following message: Do you want to recalculate the price? Yes/No. If you select Yes, the price is recalculated using the item pricing logic for the new quantity. If you select No, the price remains unchanged.


Related Topics

Cross-Referencing an Estimate to an Estimate Job

Estimating Steps