Cross-Referencing an Estimate to an Estimate Job
Cross-referencing creates a link between the estimate line and the estimate
job order. The estimates can later be copied into actual customer orders
and actual jobs.
- On the Estimate
Lines form, add a new line item to an estimate.
- On the Line Detail tab, select Job in the Reference
field.
If this item's record on the Items form has the Stocked
check box cleared and the Source Code set to Manufactured,
Job is automatically selected.
- Do one of the following:
- To cross-reference the estimate line to an existing estimate
job, enter:
- The estimate job number in the unlabeled field next to the
reference field
- The suffix (if available) for the job order in the second unlabeled
field.
- An operation number to cross-reference to a specific operation
in the third unlabeled field.
- To create a new job and:
- Assign a particular job number, enter the job number.
- Allow the system to assign a job number, leave the field blank.
- To save the record, select Actions > Save.
- Click Source.
The system displays the message "Cross-reference will be performed
from Estimate Line Item to Estimate Job."
- Click OK.
The system automatically creates the estimate job header information
and inserts the job number and the reference into the Reference
field. However, you must still create or copy the estimate job's routing.
- (Optional) Click Source again to display the cross-referenced
job.
Notice that the job's end date defaults from the estimate order
line's due date.
- To create sub-jobs for subassemblies that are cross-referenced
to the estimate order line, open the Copy
Routing BOM form.
- In the From Category field, select Current (to use
the item's current routing/BOM to create the sub-jobs; to use a different
job's routing/BOM, select Job).
- In the Copy Indented BOM field, select Yes.
- In the Item field, select the item number from which to
copy the current routing/BOM.
If you selected Job in the Category field, select
the job from which to copy the job routing/BOM in the Job field.
- In the To Category field, select Estimate Job.
- In the Job field, enter the ID of the estimate job to which
you cross-referenced the estimate line item in the previous steps.
- Click Process.
This activity copies the routing/BOM to the cross-referenced parent
estimate job and creates sub-jobs for each subassembly in the routing/BOM.
Related Topics
Copying
Routings/BOMs
Copying
a Job Order
Cross-Referencing
Demands to Supplies
Cross-Referencing
a Customer Order to a Job Order
Cross-Referencing
a Customer Order to a Project
Cross-Referencing
a Customer Order to a Purchase Order
Cross-referencing
a Job Material to a Job
Estimating Steps
Firming
Planned Orders
Job Paperwork
Report