Processing Earned Rebates
When orders that qualify for rebate programs are invoiced, earned rebate
entries are added to the Earned
Rebate Credit Workbench form, so you can process credit amounts
available for application with open credit memos.
To process earned rebates:
- Open the Earned Rebate Credit
Workbench form.
- In Promotion Code, specify
the rebate program promotion code for which to process earned rebates.
- Optionally, you can select a customer in the Customer
field, to limit processing to only that customer.
- In Application Date, specify
the date to use when creating open credit memos.
- On the Pending tab, select earned rebates to process. Only earned
rebates marked as Qualified can be selected.
NOTE:
If a rebate you need to process is not on the Pending tab, you can check
the Hold tab to see if it has been placed on hold. If so, you can set
the rebate back to Pending on the Earned Rebates
form.
- Click Process.
Open credit memos are created and the status
of the earned rebated is changed to Applied.
Related Topics
Promotion
Pricing and Rebate Programs Overview
Setting
Up Promotion Pricing and Rebate Programs
Maintaining
Earned Rebates
Closing
a Rebate Program