You can set up consolidated invoicing for a customer, a customer order, or a customer order line/release.
If you set up consolidated invoicing for a customer, all orders and lines/releases subsequently entered for the customer are marked to be invoiced with consolidated invoicing. This default can be overridden at the individual order level or line/release level.
If you set up consolidated invoicing for a customer order, all lines/releases subsequently entered under the order are marked to be invoiced with consolidated invoicing. This default can be overridden at the individual line/release level.
NOTE: The Consolidated Invoice field is enabled only if the order Status is Ordered or Planned, the order is not an EDI order, and the excise exchange setting for the order (Excs Exch field on the Tax Info tab of the Customer Orders form) is the same as the excise exchange setting for the customer (Excs Exch field on the Codes tab of the Customers form).
You can mark a customer order line for consolidated invoicing in the Customer Order Lines form. To mark a blanket order release, use the Customer Order Blanket Releases form.
NOTE: The Consolidated Invoice field is enabled only if the line/release Status is Ordered or Planned, the order is not an EDI order, and the excise exchange setting for the order (Excs Exch field on the Tax Info tab of the Customer Orders form) is the same as the excise exchange setting for the customer (Excs Exch field on the Codes tab of the Customers form).
NOTE: The Summarize Lines field is enabled only if the Consolidated Invoice field is selected, there is not more than one line of notes, and the item is not a configurable item (the Configuration Flag check box on the Items form, Controls tab, is cleared).
Consolidated Invoice Generation
Consolidated Invoices Workbench
Invalid Consolidated Invoice Records
Packages, Weight, Freight, and Miscellaneous Charges in Consolidated Invoices