A/P Vouchers and Adjustments

Use the A/P Vouchers and Adjustments form to:

Before posting these transactions, print the Voucher Transaction Report as an audit trail. To simplify your review of this report, we recommend that you enter no more than 100 transactions before posting.

If you are adding a voucher or adjustment for a vendor with a category assigned on the Vendors form, the A/P account number displays from that category. If a vendor is not assigned a category, this account number displays from the Accounts Payable Parameters form.

If the vendor's currency is different from your domestic currency, make sure that you enter the amounts in the vendor's currency (which displays under the Amounts tab).

If you are using Advanced Terms, and the voucher is not posted from Purchasing, the Advanced Terms algorithm is used to calculate the due date, based on all the elements of the terms. It is also used to recalculate the due date, if any element of the terms has changed or if the invoice date has changed. Also, display terms come from the terms code of the vendor.

When working with a voucher, you can click Distribution Generation to have the system automatically distribute the voucher for you, or you can click Distribution to display another form where you can manually distribute it.


Related Topics

Accounts Payable Steps

Creating Multi-Site Vouchers and Adjustments with the Voucher Builder

Creating Vouchers or Adjustments Automatically

Receiving an EDI Invoice (Inbound 810/INVOIC)