Creating Multi-Site Vouchers and Adjustments with the Voucher Builder

Use the Voucher Builder form to create vouchers and adjustments for multiple sites, based on the sites' PO receipts and returns:

To link multiple vouchers generated in different sites but created during one Voucher Builder generation, the generated vouchers include the originating site (where the Voucher Builder was run to create the voucher) and a Builder Voucher number. The combination of the originating site and Builder Voucher number is unique across all sites.

Requirements

Creating a Voucher Using the Voucher Builder Form

  1. Open the Voucher Builder form.
  2. Filter for a specific vendor number, name, and/or currency (or leave all of these blank to view all vendors).

    The grid then displays all received but not yet vouchered purchase orders for the selected vendors. These purchase orders are from all sites replicating the Voucher Builder category with the site where Voucher Builder is being run.

    Data displayed includes the To Site (the target site where the PO was received and where the voucher/adjustment is going to be created), Builder PO originating site and Builder PO number (if applicable), PO number, PO line/release, item, quantities, unit of measure, and so on.

  3. Specify the Type of activity to perform. By default, the form displays POs for vouchering.

    If Type is set to Voucher, the form displays all received but not yet vouchered POs for specific vendors. You can provide total material value, total freight and miscellaneous charges, and total taxes (under certain conditions as specified in the Notes below). You can also provide freight, miscellaneous charges, and total taxes (under certain conditions) against individual POs.

    If Type is changed to Adjustment:

  4. Do one of the following:
    NOTE: The grid contains all possible records for a vendor. However, after you select one record, the system automatically disables some of the other records based on the following:
    • If the first selected row has a fixed rate, then only those rows that have the same fixed exchange rate are available to be selected.
    • If the first selected row has Include Tax in Cost turned on, then only those rows where Include Tax in Cost is turned on are available to be selected.

    You can click Deselect All to clear all selected rows and start the selection process over.

  5. On the PO line/releases in the grid, you can change the received quantity (To Vch/Adj) and the Unit Cost.
  6. Include Material, Freight Miscellaneous Charges, and taxes (under certain conditions as specified in the Notes below) from the vendor's invoice in the header fields. You can enter the Freight and Miscellaneous Charges in the grid for every selected PO Line; you can enter the Sales Tax and Sales Tax2 amounts in the grid for every selected PO line that meets the criteria mentioned in the Notes below. Then, when generating a voucher all freight, miscellaneous charges, and taxes (under certain conditions) for a PO will be summed up for a target site.

    A running total for the voucher displays in the Material, Freight, Misc Charges, and tax fields below the grid. These running totals are used to verify that entered values match the vendor's invoice values you entered in the header.

    When the voucher is generated, total freight per site will be created as a single distribution. Similarly, total miscellaneous charges and total taxes will be created as individual distributions.

  7. Click Generate to generate vouchers or adjustments for the selected records. When this button is clicked:
  8. The collection is refreshed to display any POs that still need to be vouchered/adjusted for the selected vendor.
    NOTE: If the process of creating a voucher is delayed in the target site, already submitted and yet to be vouchered PO receipts may still appear in the list.
  9. Repeat the above steps to create additional vouchers or adjustments.

Notes

Error and Resubmission - Example

You click the Process button to create Builder Voucher 1 (which includes several site-specific vouchers) in SiteA for SiteA, SiteB and SiteC. If non-transactional replication is set up and the system returns an error stating that SiteB failed to create a voucher, most of the time you can just reprocess the record in SiteB's Replication Errors form.

However, if you receive the error message "Information has been changed by another user," you cannot reprocess the row. The only way to create that voucher is to recreate it, either through another session of the Voucher Builder, or manually at SiteB.

This means the voucher in SiteB will not be tied to the vouchers in SiteA and SiteC by the Builder Voucher number. Even if you use the Voucher Builder again, SiteB's voucher will have a new Builder Voucher number. However, the Vendor Invoice number can be set the same for all these vouchers, and that can be used to link all these vouchers.


Related Topics

Purchasing Overview

Creating Vouchers or Adjustments Automatically