These are the basic assumptions of unit code reporting throughout the system.
The account structure in the system is:
Account is part of the account template, unit codes are not. Any unit code can be tied to a main account, provided the Chart of Accounts setup allows that chart record access to that unit code.
On the Chart of Accounts, you can set each unit code with one of the following three attributes:
For transactions involving inventory distribution accounts, the system pulls unit codes from Item Stockroom Locations.
WIP transactions pull Acct, Unit Code 1, Unit Code 3, and Unit Code 4 from the Product Codes - WIP tab. Unit Code 2 comes from the Product Codes - General tab.
EXAMPLE: For example, a job is created for Item A. Item B is the material issued to that job. Unit Codes 1, 3 and 4 are defined on the Product Codes - WIP tab. For a job material issue, the following accounts and unit codes are used.
|
Acct |
UC1 |
UC2 |
UC3 |
UC4 |
(Debits) From Job Header WIP Accounts (Cost Detail) |
|
|
|
|
|
WIP Material |
XXXX |
XXX |
XXX |
XXX |
XXX |
WIP Labor |
XXXX |
XXX |
XXX |
XXX |
XXX |
WIP Fixed Overhead |
XXXX |
XXX |
XXX |
XXX |
XXX |
WIP Variable Overhead |
XXXX |
XXX |
XXX |
XXX |
XXX |
WIP Outside Services |
XXXX |
XXX |
XXX |
XXX |
XXX |
(Credits) From Item Stockroom Locations |
|
|
|
|
|
Inventory Material |
XXXX |
|
XXX |
|
|
Inventory Labor |
XXXX |
|
XXX |
|
|
Inventory Fixed Overhead |
XXXX |
|
XXX |
|
|
Inventory Variable Overhead |
XXXX |
|
XXX |
|
|
Inventory Outside Services |
XXXX |
|
XXX |
|
|
| Acct | UC1 | UC2 | UC3 | UC4 | |
| (Debits) From Job Header WIP Accounts (Cost Detail) | |||||
| WIP Material | XXXX | XXX | XXX | XXX | XXX |
| WIP Labor | XXXX | XXX | XXX | XXX | XXX |
| WIP Fixed Overhead | XXXX | XXX | XXX | XXX | XXX |
| WIP Variable Overhead | XXXX | XXX | XXX | XXX | XXX |
| WIP Outside Services | XXXX | XXX | XXX | XXX | XXX |
| (Credits) From Work Center of Operation (Dept. of WC) Departments record | |||||
| Direct Labor Expense | XXXX | XXX | XXX | XXX | XXX |
| Fixed Labor Overhead Applied | XXXX | XXX | XXX | XXX | XXX |
| Variable Labor Applied | XXXX | XXX | XXX | XXX | XXX |
In standard costing, variance transactions use Unit Code 2 from the Product Codes - General tab. For labor rate variance, it also uses Unit Code 1 from the Departments form. Other unit codes are pulled from the Product Codes - Variance Tab.
Customer order unit codes can be handled in one of two ways. On the Customers form there is an End User Type field. End User Type accounts can then be set up on the End User Types form. The accounts defined here are Sales, Sales Discount, Accounts Receivable, Cost of Goods Sold Material, Cost of Goods Sold Labor, Cost of Goods Sold Fixed Overhead, Cost of Goods Sold Variable Overhead, and Cost of Goods Sold Outside. If End User Type is defined on the Customers form, that type is pulled into the order and the default values for Acct, Unit Code 1, Unit Code 2, Unit Code 3, and Unit Code 4 are used from the End User Types form. If there is no Unit Code 2 on the End User Type form, it is pulled from the Product Codes - General tab.
If End User Type is not used, the system pulls the Acct, Unit Code 1, Unit Code 2, Unit Code 3, and Unit Code 4 from the Sales/COGS tab on the Distribution Accounts form for all accounts listed above except Accounts Receivable. If there is no Unit Code 2 on the Sales/COGS tab of the Distribution Accounts form, it is pulled from the Product Codes - General tab. Accounts Receivable is pulled from the Accounts Receivable Parameters form and uses all Acct, and all Unit Codes.
NOTE: See Where Unit Codes Come From for a table illustrating how unit codes are applied by activity performed.
Account/Unit Code Removal Utility