Creating and Posting Recurring Journal Entries
NOTE: Recurring journal
entries can be created in only standard or user-defined journals.
To create a recurring journal record:
- Open the Journals
form and find or create a user-defined journal.
- Select Recurring
Journal.
- Save the record.
To post recurring journal entries:
- Do one of the following:
- If you are still on the Journals
form and you have just saved the recurring journal record, click
Journal Entries. The
Journal Entries form is displayed.
- If you need to post entries for another recurring journal,
use the Explorer to open the Journal
Entries form and then find the recurring journal.
- Fill in the appropriate fields for your recurring transaction.
For a new recurring journal, you’ll need to specify all transaction
entries. For an existing recurring journal, you may only need to change
the transaction dates.
NOTE:
Transaction dates can be changed one-by-one on the Journal
Entries form, or you can change them all at once using the Ledger Posting form, which is opened
in the next step. On the Ledger Posting
form, select Single Date To All Entries
and specify the date in Date For
All Transactions.
- Select Actions > Post Journal.
The Ledger
Posting form is displayed.
Print and post the ledger.
Review the
Journal Transaction report to check for any inaccuracies.
Post the journal.
If the journal was posted before in the same period, you will
be prompted to confirm. Click Yes
to post.
After successful completion of the post, a success message is displayed
and the system returns to the Ledger Posting form.
Related Topics
About Journal
Entries
General Ledger
Overview
General Ledger
Steps