Two or more transactions are typically entered to create a balanced entry, with one transaction entered as a debit (such as receiving a cash payment), and the second entered as a credit (such as recording miscellaneous income). The sum of the debit transactions equals the sum of the credit transactions. If each group of transactions is assigned the same reference, it is easily recognizable later that these transactions were entered at the same time.
Transactions must be entered into the journal as the first step in changing an account's balance. The next step is to post the journal to the ledger, at which time the account balances are updated. After a transaction has been posted to the ledger, you cannot change it. The only way to correct an incorrect entry is by entering a reversing entry.
You cannot directly delete a ledger transaction; however, you can enter a journal transaction for an opposite amount (and the same date as the original transaction), and then post that transaction to the ledger to cancel out the previous transaction.
SyteLine initially creates the following system journals, which you cannot delete:
Except for unit codes, the distribution journals are read-only. The General Journal and any user-defined journals are considered "writeable". Transactions for the distribution journals are entered from the appropriate SyteLine function.
EXAMPLE: After a payment is entered and posted through Accounts Payable, the transaction appears in the A/P Dist Journal. Transactions for the General Journal are entered through the General Ledger.
You can also update unit codes for a journal transaction residing in a read-only journal.
A standard journal may be set up for recurring transactions (such as rent, mortgage, payroll, or loan payments). When transactions are posted from the General or standard journals, there is an option available to delete all entries in the journal.
Do not delete recurring entries in the standard journals. The transactions are needed for the next period's posting. Recurring entries are usually the only entries in user-defined journals you would not delete.
The entries in the General Journal change from period to period and need to be deleted.
Creating Auto-Reversing Transactions
Creating a User-Defined Journal
Creating and Posting Recurring Journal Entries
Deleting a User-Defined Journal
Importing Journal Entries from External Sources