Entering Customer Payments
To enter and process payments from customers, use the A/R Payments
form. On this form, enter payments for invoiced amounts, finance charges,
and other amounts your customers owe you.
NOTE: You can enter
and post non-customer payments to the General Ledger as non-A/R cash.
To create a payment, on the the A/R
Payments form:
- Select Actions > New.
- Enter the appropriate information in the following fields:
- Customer - Select the customer
ID of the customer the payment is for.
- Type - This field displays
the customer's default payment method, but you can select a different
method.
- Number - Enter the check
or draft number of the payment.
- Receipt Date - Enter the
date you received the payment, or accept the default, which is
today's date.
- Payment Due Date - (Available
only if the payment type is Draft.) Enter the date the
draft is due.
- Deposit Date -Enter the date
you deposited the check. This field is available for entering
post-dated checks. It is enabled only if the payment type is Check,
and no credit memo is associated with the payment. Enter the date
on the customer's check.
- G/L Reference Enter a reference
ID to appear in the distribution journal for this transaction,
or accept the default, which is ARP followed by the check
or draft number.
- Description - Enter a description
to appear in the distribution journal for this transaction, or
accept the default description.
- Bank Code - This field displays
the customer's default bank code, but you can select a different
code for the bank into which the payment will be deposited.
- Customer Amount - Enter the
amount of the payment.
- Select Actions > Save.
You can then distribute
and post the payment.
Related Topics
Accounts
Receivable Steps
Creating Open
Payments for a Customer
Distributing
Customer Payments
Entering
Customer Payments Using A/R Quick Payment Application
Importing
A/R Payment and Distribution Data from Bank Files
Posting Payments