Entering Customer Payments Using A/R Quick Payment Application
To process payments from customers, you can use the A/R
Quick Payment Application form. You can select open invoices,
finance charges, payments, and credit memos.
To process payments using the A/R
Quick Payment Application form:
- Select Actions > New.
- Enter the appropriate information in the following fields:
- Customer - Enter the customer
ID of the customer you're entering the payment for.
- Type - This field displays
the customer's payment method by default, but you can select a
different method.
- Number - Enter the check
or draft number for this payment.
- Receipt Date - Enter the
date you received the payment, or accept the default, which is
today's date.
- Payment Due Date - (Available
only if the payment type is Draft.) Enter the date the
draft is due.
- Deposit Date - Enter the
date you deposited the check. This field is available for entering
post-dated checks. It is enabled only if the payment type is Check,
and no credit memo is associated with the payment. Enter the date
on the customer's check.
- G/L Reference Enter a description
to appear in the distribution journal for this transaction, or
accept the default, which is ARP followed by the check
or draft number.
- Description - Enter a description
to appear in the distribution journal for this transaction, or
accept the default description.
- Bank Code - Enter the bank
code of the bank from which the payment will be made, or accept
the customer's default bank code.
- Amount - Enter the amount
of the payment.
- Select Actions > Save.
NOTE: You must
perform this step before you can select any transactions in the grid.
All open invoices, finance charges, payments, and credit memos for
this customer display in the grid at the bottom of the form. If any
of these transactions have been distributed, the Selected check
box is selected for each.
NOTE: On the
A/R Quick Payment Application form, non-A/R payment distributions
display as selected in the grid. The amounts display in the
Discount and Allowance columns. In the Discount
column, you enter Credit Amount 1, and in the Allowance
column you enter Credit Amount 2.
- For each transaction you want to make a payment against, select
the Selected check box, or, to select all the displayed transactions,
click Select All.
- Select Apply. The system displays a message informing you
of the actions that were taken.
Related Topics
Accounts
Receivable Steps
Creating
Open Payments Using A/R Quick Payment Application
Entering
Customer Payments