Setting Up Multiple Financial Sets of Books
To set up a multi-FSB, follow these steps:
- On the General
Parameters form, select Multiple
Financial Sets of Books.
- If this set of books will use a currency that is not already set
up in SyteLine, use the Currency
Codes form to add the new currency.
- On the
Multi-FSB Accounting Periods
form, create a fiscal calendar for the new set of books.
- On the Multi-FSB
Charts form, specify a name and description for the chart
of accounts for this set of books.
- Save the record.
- Add accounts to the new chart of accounts, either automatically
or manually.
- To add accounts automatically, click Copy
COA on the Multi-FSB Charts
form. This opens the Multi-FSB
Copy Chart of Accounts form so you can copy the standard
GL chart of accounts for the new set of books.
- To add accounts manually, use the Multi-FSB
Chart of Accounts form. See Maintaining
the Multi-FSB Chart of Accounts.
- On the Multi-FSB Charts
form, click Confirm Mapping
to run a check on account mapping. A message is displayed to let you
know if there are any problems. If successful, the
Accounts Mapped option is selected automatically.
- On the Multi-Financial
Sets of Books form, define the new set of books with this
information:
- FSB: Specify a name
and description for the new set of books.
- FSB COA: Select the
chart of accounts created above.
- Fiscal Calendar: Select
the fiscal calendar created above.
- Currency: Specify the
currency to use for this set of books.
- CTA Account: Select
the account to use for recording debits and credits that may occur
to rebalance the Multi-FSB ledger due to currency conversion during
general ledger posting. This is necessary only if the selected
Currency is not Domestic.
- Save the record.
- If you need beginning balances for the multi-FSB ledger, use the Multi-FSB Journal Entries form
to enter them manually and then post them.
- To activate the new financial set of books for use, select Active on the
Multi-Financial Sets of Books form. Once active, the multi-FSB
receives all posted GL ledger transactions, regardless of the date.
If you select Compress Ledger,
ledger records for this set of books are compressed automatically
by date, account, and unit code. For additional flexibility, you can
use the Compress Multi-FSB Ledger
Transactions utility to set different compression options and
process the compression.
Related Topics
Deleting
Multi-FSB Records
Maintaining
the Multi-FSB Chart of Accounts
Multiple
Financial Sets of Books Overview
General
Ledger Setup
About
Accounting Periods