Currency Codes

The Currency Codes form maintains currency codes, symbols and formats entered for use in the system.

If you do not have existing currencies already defined in SyteLine, we recommend that you use ISO currency codes (available through the drop-down menu on the Currency field) when defining new currencies.

For information about mapping ISO 4217 currencies to existing currencies, see Mapping ISO 4217 Currencies to Existing Currencies.


Related Topics

Multi-Currency Overview

Multi-Currency Setup

Setting Up the Euro Currency Code

Using Input Masks to Set Up Field Formats

About Realized and Unrealized Gains and Losses

ISO Currency Codes