Voiding a Posted Check Manually
Three procedures allow you to void, or back out of,
transactions. The following procedure is for manually voiding a single
posted check. For more information about the other two procedures, see
the following:
To void a posted check manually:
- Open the Payroll
for Pay Period form.
- Enter the employee number.
- In the Check Type field, select Manual.
- Open the Payroll
Processing form.
- Update the form with negative amounts, to "back out"
the entries made by the payroll run. Be sure to fill in any necessary
information on all tabs: Pay, Tax, and D & E.
- Post the payroll transaction, using the
Print/Post Payroll Checks
form.
Related Topics
Payroll Overview
Payroll Procedures
Payroll Setup