Three procedures allow you to void, or back out of, transactions. The following procedure is for voiding a specified range of posted payroll checks. For more information about the other two procedures, see:
NOTE: Use the following procedure to void checks that have been posted.
To void a specified selection of posted checks:
After you select the range of checks, you can select individual checks for the void action. So, if you have multiple but not continuously numbered checks to void, you can enter in these fields the lowest check number and the highest check number, and then later select only the checks you actually want to void.
The system displays all posted checks within the range.
NOTE: You cannot select the Commit option until after you have selected Preview and then clicked Process.