Voiding Checks in a Pay Period
Three procedures allow you to void, or back out of, 
 transactions. The following procedure is for voiding unposted checks within 
 a specified pay period. For more information about the other two procedures, 
 see:
NOTE: The following 
 procedure can be used if you have printed checks but have not posted 
 them.
To void a specified range of unposted checks:
	- Open the Print/Post Payroll Checks 
	 form.
 
	- In the To Print/Process group box, specify the bank, starting 
	 check number, date of issue, and type of form to use when printing 
	 the report.
 
	- (Optional) To include zero-amount checks, select the Print Zero 
	 Amount Checks check box.
 
	- In the Employee Type group box, select which types of employees 
	 to include in this action.
 
	- In the Starting and Ending Department fields, select 
	 the starting and ending departments for the checks to be voided, or, 
	 to void checks for all departments, leave both fields blank.
 
	- In the Starting and Ending Employee fields, select 
	 the first and last employees whose checks are to be voided; or, to 
	 void checks for all employees, leave both fields blank.
 
	- Select Void Check(s).
 
	- Click Process.
 
NOTE: If you have 
 already run the Final Register and Post option for the specified 
 checks, run the Void 
 P/R Posted Payments utility.
Related Topics
Payroll Overview
Payroll Procedures
Payroll Setup