The due date for the selected item displays. The system uses the following fields to determine the due date:
| Type of order | Field used to determine Due Date |
|---|---|
| MRP or APS | The Date field on the Master Planning Display form. |
| Item Replenishment | Today's date plus item's lead time. |
| Order | The Due Date field on the Customer Order Lines form. |
| Project | The Effective Date field on the Project Tasks form. |
| Transfer | The Scheduled Ship Date field on the Transfer Order Line Items form. |
| Job | The Start Date field on the Job Operations form. |
NOTE: The due date must be a valid manufacturing day. The manufacturing day (or MDAY) calendar is a list of valid manufacturing days between the MDAY Start and MDAY End date fields on the Planning Parameters form, using the default scheduling shift and Holiday definitions to generate the list.