Setup Rule
Select the rule that determines when to set up the operation.
- Always: Always apply setup time prior to processing the load.
- Basis: Apply setup only when the item or setup group from the previous operation was different than the one this operation is processing (using this resource). Select Item or Setup Group in the Setup Basis field.
- User-defined (3-39): base setup on a user-defined rule. See Writing a Custom Scheduler Rule for more information about creating user-defined rules.