Setup time is the portion of the operation spent preparing the resource for performing the operation (such as tooling, proofing, or any other work not proportional to the units produced). The system factors the setup time into the duration of the operation.
Depending on your type of business, resources may always need to be set up. Or, they may need to be set up only when changing from working on one type of item to another. Likewise, the setup time could be a fixed value or it could vary depending on the type of item.
In APS and in the Scheduler, when you post setup time against a job with a job transaction, APS and Scheduler consider the posted time and plan or schedule the operation using the adjusted setup hours. For example, if the normal setup time on an operation is 10 hours, and you post setup time of 3 hours against the job/operation, the operation will be planned and/or scheduled using 7 hours.
APS uses only the Setup hours value specified on the Standards tab on the Operations form, divided by Efficiency (also specified on the operation). This value is intended to be an average setup time. The Scheduler uses a more detailed setup value, which the rest of this help topic describes.
On the operation, in the Setup Resource Group field, define a resource group from which to allocate the resource to be set up. The Scheduler will use the resource allocated from this group to determine the setup time based on the criteria you define (described later in this help topic). If you leave the Setup Resource Group field blank, the operation incurs no setup time.
NOTE: The Scheduler loads the calculated setup time onto all resources allocated to the operation. For example, if the operation allocates three resources, one of which is the setup resource, and the calculated setup time is 1 hour, all three resources are loaded with 1 hour of setup time.
To specify the situations in which the operation requires the resource to be set up, select the appropriate Setup Rule on the operation record:
When the Setup Rule field is set to Basis, select the appropriate Setup Basis on the operation record:
NOTE: Each operation can have only one setup basis, but you may define many setup basis configurations. For example, the bike assembly operation could have a setup basis of "Type of Handle Bar," and the bike frame operation could have a "Color" basis.
You can define a fixed setup time or use a calculated value. You can select the Setup Time Rule on the operation record to represent either situation.
See Setup Time Example for an example of the possible combinations of setup rules and setup time rules.