This form is used only with the APS planning mode.
Use this form to view the utilization and load for a specific resource at various points in time. This form does not display any information until you run the Planning activity.
Each row in the grid next to the graph displays a single interval in time for the resource, based on the setting of the Intervals field. The intervals are listed in chronological order. Use the built-in scroll bar to display data for additional intervals.
The graph shows the resource load profile for the record selected in the grid (this is the percentage of the resource's on-shift hours that are being utilized). If there are no load hours for a given interval record, no graph will display for it.
The Actions menu includes the option Go to Resource Plan, where you can view details about the work this resource will process.