Containers Overview

The containers functionality allows inventory to be grouped into containers within a warehouse and stockroom location. The container is assigned a unique container ID. Incoming inventory can be added into a container. Internal inventory movement and outgoing inventory can be transacted at the container level. These transactions allow you to provide a container ID, and the system will perform all the single-level inventory transactions transparently, allowing inventory movement to be performed with a single transaction.

Note: In order to receive inventory into a container, the receive quantity must be greater than or equal to 0, and the on hand balance must be greater than or equal to 0.

Transaction Types

Add Inventory

You can add inventory to a container through the following transactions:

Bulk (Inventory Removed)

You can remove inventory from a container through the following transactions:

Other Considerations

Create a Container

Use the Containers form to create a container.

Utility Forms

Compare Container To Customer Order Utility

Compare Container To Project Resource Utility

Report Form

Container Contents Report

Query Form

Item Containers Query


Related Topics