You can create manufacturing job orders by creating them manually on the Job Orders form, by cross referencing from a customer order line, by firming a planned order, or by running the Copy Routing/BOM utility. A job order has a Start and End date that the system calculates or you enter manually depending how you create the job:
The Start and End dates may determine when the system plans the job's materials and are used as input values to the Scheduling activity's calculations.
The job also has a Projected date, which the APS Planning activity or Scheduling activity calculates based on the latest plan information. Depending on the setting of the Planning Analysis for Non-Scheduled Jobs parameter, you will use either the Start/End dates or the Projected date for your output analysis activities.
This topic describes how the system updates a job's Start, End, and Projected dates differently depending on how you created the job and depending on the planning mode you are using. It also describes how the system uses these dates on the output forms and reports.
The conditions that determine how a job's dates are set depend on whether you are using the MRP or APS planning mode.
The APS Planning activity calculates job dates as follows:
The Scheduling activity populates or updates the Projected date, but never populates the Start and End dates.
The table below summarizes the conditions when APS Planning or the Scheduling activity updates the job dates.
| Date | APS Planning | Scheduling |
|---|---|---|
| Start/End | Updates if dates are blank | Never updates (because the APS Planning activity will already have populated the Start and End dates) |
| Projected | Updates if job is not Scheduled | Updates |
MRP Planning does not populate a job's blank Start and End dates, nor does it modify existing Start and End dates. MRP also does not populate or modify a job's Projected date field. If you are using MRP, you must run the Scheduling activity to populate any of the job dates.
The table below summarizes the conditions when MRP Planning or the Scheduling activity updates the job's dates.
| Date | MRP Planning | Scheduling |
|---|---|---|
| Start/End | Never updates | Updates if dates are blank and job was completely scheduled |
| Projected | Never updates | Updates |
Either the job's Start and End dates or the Projected date may appear with the job on output forms (such as Planning Detail and Material Planner Workbench) and reports (such as the Order Action Report), depending on the following conditions:
The table below summarizes the conditions that determine how output forms and reports display job dates when you are using APS mode.
| Job Scheduled? | Use Scheduled Times in Planning | Planning Analysis for Non-Scheduled Jobs | Dates Used |
|---|---|---|---|
| No | No | Use Job End Date | Job Start/End |
| No | No | Use Projected Date | Projected date |
| No | Yes | Use Job End Date | Job Start/End |
| No | Yes | Use Projected Date | Projected date |
| Yes | No | Use Job End Date | Job Start/End |
| Yes | No | Use Projected Date | Projected date |
| Yes | Yes | Use Job End Date | Projected date |
| Yes | Yes | Use Projected Date | Projected date |
In MRP mode, if the job is NOT scheduled, the job's Start and End dates are always used on the output forms and reports.
If the job is scheduled, the Use Scheduled Times in Planning parameter determines which dates are used. If Use Scheduled Times in Planning is selected, the job's Projected date is used. If Use Scheduled Times in Planning is cleared, the job's Start and End dates are used.