This topic describes how APS plans safety stock replenishment. See MRP Overview for a description of how MRP plans safety stock.
APS will plan to keep inventory at or above safety stock. When safety stock is set up correctly, the system will generate ONE safety stock replenishment order for any item that drops below safety stock with the following attributes:
For purchased Items:
Due date = Date & Time of APS plan + Lead time (using the PCAL shop calendar)
Lead time = Fixed + Dock-to-stock + Paperwork lead times
For manufactured items:
Due date = Date & Time of APS plan + Lead time, using the PCAL shop calendar
Lead time = Fixed + Dock-to-stock + Paperwork + (Variable * Safety Stock level).
Note: The safety stock level in the lead time formula for manufactured items is the total level you are attempting to maintain (as shown in the Safety Stock field on the Items form), and not the shortfall amount when on-hand dips below safety stock.
When you run APS Planning, the system plans safety stock replenishment for manufactured items according to one of two processes: Post Process or Dynamic. The system automatically selects which process to use for an item based on either the relationship between Order Minimum and Safety Stock Level, or the relationship between Order Multiple and Safety Stock Level.
| If the Order Minimum/Order Multiple (whichever is greater) is... | The system uses this behavior... |
|---|---|
| Greater than Safety Stock | Dynamic |
| Less than or equal to Satefy Stock | Post Process |
During the APS planning run, as each demand is planned, the item's safety stock level is evaluated. If a demand causes safety stock to dip below the safety stock level:
Once safety stock is planned for an item using dynamic behavior, the Time Fence is turned off. Time Fence is no longer needed since the Safety Stock Order protects the safety stock quantity.
After all demands, or orders, are planned, the system plans safety stock for each item in order by Low Level Code, from low to high. For each item, if the inventory falls below the safety stock level, outside of the time fence, the system creates a Safety Stock plan at the point in time with a quantity equal to the difference between safety stock level and the lowest projected inventory level outside of the Time Fence.
For manufactured items, it is possible that in some situations (when you have demands due far into the future that use up your near-term supplies), the system may generate a safety stock planned order that is due much earlier than the demands need it, leaving you with a large quantity of unnecessary supplies.
To avoid this problem, we recommend you set the Time Fence Rule to Accumulated Lead Time for the item on the Items form. By setting this Time Fence Rule, the later demands will not use the near-term supplies and the system will create planned orders due closer to when the demands are actually due.
After the system finishes planning all the demands normally, according to order priority, it performs a second, time-phased planning run. At the current date and at every date where there is a demand for the item, the system compares the on-hand quantity with the safety stock value:
Once the level is at or above safety stock, demands due later than the current date + standard lead time cannot reduce the level back below safety stock.
NOTE: The system generates only a single safety stock planned order for a given item (it does not generate a planned order for each instance where the on-hand level drops below safety stock).
The system plans safety stock for transferred items the same way it plans safety stock for purchased items.
The following parameters appear on either the Planning Parameters form (and affect ALL items) or on the Items form. They either affect the way the system generates planned orders to replenish safety stock or the system uses them along with the safety stock value to calculate a value used for another feature.
| Parameter | Appears On |
|---|---|
| Consider Negative On Hand | Planning Parameters |
| Preservation Level Multiplier | Planning Parameters |
| Suspend Time Fence (Second Pull) | Planning Parameters |
| Order Minimum | Items |
| Time Fence Rule | Items |
| Time Fence Value | Items |
Reorder Point items are usually inexpensive, high-volume items (such as nails, bolts, etc.) that you want to track and replenish differently than normal items. The system does not generate safety stock replenishment planned orders for Reorder Point items. However, the "On Hand below Safety Stock" exception is generated when the system creates a reorder-point planned order. See the Reorder Point topic for more information.