Assigning New Serial Numbers
When a quantity of a serial-tracked item is added to inventory through 
 a receipt, you must assign serial numbers for each item received. This 
 is handled on the transaction form's Serial Numbers tab.
You can optionally preassign serial numbers for a particular purchase 
 order, transfer order, or job transaction. For more information, see Preassigning Serial Numbers.
	- In the transaction form, enter the item number, quantity, and any 
	 other required information (such as location). The Serial Numbers 
	 tab is activated, which indicates that the item is serial-tracked.
- In the Serial Numbers tab, the Target Qty and Generate 
	 Qty default to the value of the Quantity field in the Detail 
	 tab. If necessary, change the Generate Qty. It should indicate 
	 how many serial numbers you want to generate and move to inventory.
- Create new serial numbers, up to the quantity of the item. Use 
	 any of these methods: 
	
		- In the grid, enter new serial numbers. Use any prefix and field 
		 format, up to 30 characters.
- To generate a range of serial numbers, click Generate. 
		 The system starts the generated serial number list by using the 
		 next sequential serial number, and continues generating numbers 
		 until the item's quantity is reached. You can then change the 
		 generated serial numbers. (The Generate button is enabled only 
		 if the Expand S/N field is selected in the Inventory 
		 Parameters form.) 
- For preassigned serial numbers, you do not need to click Generate. The grid displays 
		 all unreceived preassigned serials, and a number corresponding 
		 to the quantity being received is displayed automatically. However, 
		 you can generate new serial numbers if you want to, instead of 
		 using the preassigned ones.
- Use a combination of generated and manually created serial 
		 numbers.
 
- In the grid, select or deselect the serial numbers to use for the 
	 transaction. If you deselect a row in the grid, it is deleted.
- When you process the transaction, the selected serial numbers are 
	 included with the transaction. When the transaction status is "complete" 
	 or "closed," any preassigned numbers that are not used go 
	 back into the pool for use with another transaction if the prefix 
	 matches.
- To specify other information about a new serial number, use the 
	 Serial Numbers form.
NOTE: To create new 
 system serial numbers for a Vendor Ship Notice (GRN) where vendor-assigned 
 serial numbers exist, use the Vendor Serial button instead of the 
 Generate button. Vendor-assigned serial numbers come into the system 
 only through EDI transactions.
Related Topics
Setting 
 Up Serial Number Processing
Preassigning Serial 
 Numbers
Tracking 
 Serialized Materials
Defining 
 Intelligent Lots and Serials