This process describes how to create a manufacturing job order manually on the Job Orders form. Only required fields and tips regarding selected optional fields are discussed in this procedure. For more information, including descriptions of all fields on the form, see the field help topics for the Job Orders form.
NOTE: The system provides several methods for creating job orders in addition to this method. See the "How-To" link above.
By default, the system uses the next unique number. If you allow the system to assign the next job number, the job number does not display in the job number field until you save the new job.
You can set up a global prefix, Job Prefix, on the Shop Floor Parameters form to display a sequential number.
By default, the system uses the current system date. This means that you do not need to change this field unless you want the job's creation date to be different than today's date.
The revision number helps you track which, of a number of revisions authorized through Engineering Change Notices, the transaction affects. If the status of the job order is Firm, the Revision field must be validated.
NOTES: If the Start or End date falls on a weekend and Saturday and Sunday are not defined as manufacturing days, the system automatically adjusts the date to reflect a weekday.
The Projected date is entered automatically when you click the Get ATP or Get CTP button or when you run the planning or scheduling activities.
You can now add a routing and bill of material to the job.
Cross-Referencing a Customer Order to a Job Order
Cross-Referencing a Customer Order to a Project
Cross-Referencing a Customer Order to a Purchase Order
Cross-referencing a Job Material to a Job