Creating APS Alternatives
		
	An alternative is a container for specific data to drive APS and Scheduling. 
 Each alternative represents a "what if" scenario to analyze. 
 You must always have a productionalternative, which is alternative 
 "0." The alternative 0 references your SyteLine 
 application data that you interact with on other forms. The APS Planning 
 and Get 
 ATP/CTP processes use the data in alternative 0.
To investigate possible changes to your process, you must create one 
 or more planning alternatives (such as alternative 1, 2, 3, etc.) 
 in addition to the production alternative.
Creating the Production Alternative
SyteLine 
 provides a blank alternative 0; you must enter the information to reference 
 your data.
	- Open the APS 
	 Sites and Alternative Management form.
- Select Actions > New. 
- In the Alternative field, 
	 enter 0.
- In the Planning Site field, 
	 select the SyteLine 
	 site you are defining.
 If you have multiple SyteLine sites that will be included in global 
	 planning, you must create a separate alternative record for each 
	 site. That is, if you have two sites, A and B, you must create an 
	 alternative 0 record for site A and a second alternative 0 record 
	 for site B.
- In the Priority field, 
	 enter the sequence number of this site for global planning. 
 When you run APS Planning in global mode, the system plans the site 
	 with the lowest Priority number (00) first.
- If this is the alternative 0 record for the local site (that 
	 is, the site at which you're actually entering the record), in the Type 
	 field, select Local. If this is the alternative record for 
	 one of the other sites in your environment, select Remote.
- In the APS Server Service Host 
	 Name field, enter the name of the machine where the Planning 
	 and Scheduling Service is running. 
 This is typically the SyteLine 
	 utility server. See the Infor SyteLine Installation Guide 
	 for instructions on installing the Planning and Scheduling Service.
- In the APS Server Service Port 
	 field, enter the port number on which the Planning and Scheduling 
	 Service is installed and running.
 If you do not remember the number of the port on which you installed 
	 this service, open the Windows Services applet (Start 
	 > Programs > Administrative Tools > Services) on the 
	 SyteLine utility server and look for "Infor APS Server"; 
	 the port number will be listed along with the service name.
- In the Planner Database Host Name 
	 field, enter the name of the machine where the planner database is 
	 running. 
 For instructions on installing and starting planner databases, see 
	 the Infor SyteLine Installation Guide.
- In the Planner Database Port 
	 field, enter the port number on which the planner database is running. 
	 
 This field associates the production alternative with the planner database 
	 in which the actual planning calculations are performed. This planner 
	 database must be running when you perform the Get ATP/CTP process 
	 or run APS Planning. For information on creating and starting a planner 
	 database, see the Infor SyteLine Installation Guide.
- In the SQL Host Name field, 
	 enter the name of the machine where the SQL Server is installed. The 
	 Planning and Scheduling Service uses this information to connect to 
	 the SyteLine application database.
- In the SQL Database Name 
	 field, enter the name of your SyteLine application database.
- In the Timeout field, enter 
	 the number of seconds for the system to wait for a response from a 
	 remote site when running APS Planning in global mode. Make sure the 
	 Timeout value is sufficient--we 
	 recommend at least 60 seconds.
- Select Actions > Save to save the parameters. It takes 
	 several minutes for the save process to complete.
Repeat these steps to enter a production alternative record for each 
 site in your environment.
Creating Alternative Plans
		To create a planning alternative, follow the steps listed above for 
 creating the production alternative, and change the steps as follows:
	- In the Alternative field, 
	 enter a new number for the planning alternative (such as 1 
	 or 2).
- In the Planner Database Port 
	 field, enter the port number for a different planner database than 
	 the one you specified for the production alternative (make sure to 
	 first create and start an additional planner database for this alternative 
	 as described in the Infor SyteLine Installation Guide). 
	 Each alternative must reference a separate planner database.
Copying Production Data to a Planning Alternative
After creating an alternative plan, select the new alternative and click 
 Copy/Refresh to copy the data 
 from alternative 0 (the production alternative).
Related Topics
APS Overview
Planning Parameters