Use the Planning Parameters form to enable features and options used throughout the MRP, APS, and MPS planning functions. Changing these parameters does not affect the plan until you run APS Planning, MRP Planning, or the MPS Processor (depending on the parameter).
When the planning mode is MRP, the APS and Advanced APS tabs are disabled.
Using a Master Production Schedule