Cross-Referencing a Job Material to a Purchase Order
Use the Job
Materials form to cross reference a job material to a purchase order.
- On the Job Materials form, add a new material or select an existing
one.
- Select the Source tab.
- Make sure Purchase Order is selected in the Ref field.
- To cross-reference the job material to an existing purchase order,
enter the PO number in the unlabeled field next to the reference field.
In the second unlabeled field, enter the PO line number (or leave
it blank to create a new line on this PO).
To create a new purchase order and assign a particular PO number,
enter the PO number. To create a new purchase order and allow the
system to assign a PO number, leave the field blank.
- Click the Source button. The system creates a purchase order
and purchase order line that is cross-referenced to the job material
and inserts the PO number into the Reference field.
- Optional: You can click Source again to display the cross-referenced
purchase order line.
NOTE: You can cross-reference
to a range of purchase orders using the Material
Planner Workbench form.
Deleting or Updating the Cross-Reference
After a cross-reference is created, you can change it by either removing
the line item or changing the cross-reference information, thus deleting
the cross-reference. When this happens, the system displays a warning
message indicating the cross-reference will be unlinked.
To view unlinked references, you can filter on the Unlinked
Reference check box. You can then do one of the following:
- Clear the Unlinked
Reference check box so that the record is no longer unlinked.
There is no indication in the system that the record was ever cross-referenced.
- Delete the supply record.
- Leave the Unlinked Reference check box selected.
Related Topics
Receiving
Cross-referenced Items